STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

ETB/MTB activation on STM32WB55

Hello,I have a question concerning STM32WB55 MCU. We are using it, and use SWD as debug, without advanced debug features (traces).We are now facing complex bugs, and I would like to activate traces on that MCU for the M4 Core.We do not have TRACE pin...

STM32WL I2C recovery after stop-2 sleep mode

We have STM32WL working well on LoRa together with Teseo-liv3f Nucleo boards. We now need to have it to sleep for low power between tasks.Our software is based on the LoRaWAN_AT_Slave example. In there we can allow everything to go into sleep mode 2....

Darcy1 by Associate II
  • 1698 Views
  • 1 replies
  • 0 kudos

Update connection interval update fails

Hi all,Im using the STM32WB as client to send some measurement data to my phone or pc application. Communication works fine and now I'm trying to reduce the power a bit and want to change the connection interval to high when I'm sending much data.I'm...

Taxara by Associate III
  • 989 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.