STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

0x20008000 or 0x20009000?

I am using the LoRaWAN end-node dual-core demo on an STM32WL5M.  I noticed the RAM_SHARED section in the .LD files of each core project points to different addresses, one to 0x20008000 and one to 0x20009000.  Is this a potential issue?

Resolved! need help in MCU selection regarding Bluetooth

Dear esteemed members,I am designing a Bluetooth based small headset kind of application, which will be capable ofreceiving audio stream, streamed through a device like mobile or any other.also need to control few GPIO with mobile, command will be se...

Preet by Associate II
  • 839 Views
  • 5 replies
  • 5 kudos

Resolved! issue with RTC Calendar alongside BLE on STM32WB

Hello,I’m working on a project with the STM32WB55 where I use BLE (which is working fine) and also want to use the RTC Calendar. The project was generated with STM32CubeMX, RTC is using LSE.The problem:The RTC calendar runs, but its time counting is ...

DPiór.1 by Associate III
  • 815 Views
  • 2 replies
  • 0 kudos

Ble disconnection event 0x3E

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code Hi All, I’m developing a custom BLE Central + ...

STM32WL5MOC blank application

Hi,I made a custom board with a STM32WL5MOC module and I want to test LoRaWAN connectivity. How to get a blank example for testing LoRa? I try to use the End_Node example of the B-WL5M-SUBG1 board, but it requires some environmental sensors to be ini...

Auto-Reset Failure After Flashing STM32WLE5JC

Hello, I’m facing an issue with the STM32WLE5JC controller after flash programming. After programming, the controller does not automatically reset. It only starts working after manually turning the power OFF and ON. In these cases, I've observed the ...

suriya by Associate II
  • 586 Views
  • 0 replies
  • 0 kudos

Resolved! Low power Bluetooth advertising with STM32WB5MMG

The goal of my program is to:          1. Set low power time that runs off HSI for 10 seconds          2. Enter stop2 WFI           3. Wake up from low-power interrupt          4. Advertise for 5 seconds            5. Stop advertising          6. Rep...

aidant by Associate II
  • 909 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.