2025-08-31 11:20 PM
Hello,
I’m working on a project with the STM32WB55 where I use BLE (which is working fine) and also want to use the RTC Calendar. The project was generated with STM32CubeMX, RTC is using LSE.
The problem:
The RTC calendar runs, but its time counting is incorrect.
Instead of incrementing one minute (60 seconds), it only increments 4 seconds per minute.
What I tried:
In main.cpp, during RTC initialisation:
hrtc.Init.AsynchPrediv = CFG_RTC_ASYNCH_PRESCALER;
hrtc.Init.SynchPrediv = CFG_RTC_SYNCH_PRESCALER;
Has anyone experienced this before on STM32WB55? Any guidance or hints would be greatly appreciated.
Solved! Go to Solution.
2025-10-06 4:52 AM
Thanks for the info @STTwo-32
Actually RTC Calendar is working good now :) I don't know why, I don't remember what I changed.
2025-09-25 9:51 AM
Hello @DPiór.1
On the BLE context, Since the RTC is used for the HW timers. It may be some bad behaviors will using RTC Calendar modes. So, i may recomand you to use the Timer server utility for your application. Part 4.5 of the AN5289 Rev 18 may also help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-06 4:52 AM
Thanks for the info @STTwo-32
Actually RTC Calendar is working good now :) I don't know why, I don't remember what I changed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.