STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

the user button code is not working on NUCLEO-WB55RG

I am trying to use the pushbutton of NUCLEO-WB55RG and I tried coding it in both external interrupts and also as a gpio input. The pin configuration is correct. The same code is running on other Nucleo boards such as L496 and L432. But the code does ...

PMana.1 by Associate II
  • 800 Views
  • 1 replies
  • 0 kudos

How to transmit the 247 data in stm32wb?

I have configured the stm32wb with 247 data transmission but in the receiver side the buffer seems like it transferred only 20 bytes in the notification. For note: The values are updated in the 255 sized cmd_buffer in the aci_gatt_update_char_value(...

SKuma.24 by Associate II
  • 1536 Views
  • 2 replies
  • 0 kudos

STM32WLE timing between OTAA request and gateway response

Hi All,I'm creating a TTN application using a STM32WLE5JC. After configuring the LoRaWAN application in STM32CubeIDE I have been able to send an OTAA join request to a gateway using the credentials provided by the TTN application. I can see the join ...

moatjon by Associate III
  • 958 Views
  • 0 replies
  • 0 kudos

How sequencer works in stm32wb

I don't understand if a function that you have set in the sequencer goes out of the sequencer once it has been executed or you have to do it with code. I have read AN5289 and I didn't find out the answer. Thanks in advance.

CGali.2 by Associate III
  • 959 Views
  • 0 replies
  • 1 kudos

STM32WB55 FREERTOS Example:

I am using STM32WB55 HeartRate FREERTOS Example. But when I do something in the Task, it runs only once though it has a while 1 Loop. Can anyone guide me with that?Thanks in Advance.

Warning device under test not responding...

Using the STM32WB55CG (USB dongle) with the P-NUCLEO kit.STM32CubeMonitor-RF on my win10 will not detect the COM I am using. I updated the FUS, BLE_stack, FW as described using STM32CubeProgrammer 2.8.0.UM228 says something about VCOM drivers, how do...

DS.4 by Senior II
  • 1039 Views
  • 1 replies
  • 0 kudos

Hi, I am doing Stm32wb55, transmitting data sets from Main board to dongle. Is there anyway that I can display the data in dongle on my computer.

Because the dongle is a USB and I am not sure how to move the data to computer. Do I need another main board and transmit data from dongle to the main board again? Or is there a simple way that I can directly access the data in dongle?Looking forward...

NDong.2 by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

Connect to STM32WB Via Android Programmatically

Hello!I'm trying to build an Android app to connect to my STM32WB device using a custom BLE profile.I'm able to connect and interact with my device via the ST BLE Toolbox app, but when I try to create a Bluetooth socket within Android studio and conn...

WSher.1 by Associate II
  • 959 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.