STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

How to update beacon data on STM32WB55?

I have created a project in CubeMX with CubeWB. Set the device to beacon mode (UID). On initialization, I can set the NamespaceID and BeaconID. But I do not understand how I can change this data during the operation of the beacon. Please tell me the ...

NKcin.1 by Associate
  • 993 Views
  • 0 replies
  • 0 kudos

BLE disconnection issue on STM32WB5MMG

I am using BLE peripheral on STM32WB5MMG module. For some reason the BLE gets disconnects on its own and not able to connect it again when it disconnects on its own. So I want to understand on what event BLE gets disconnects. Is it anyway possible to...

0693W00000FDrOCQA1.jpg
Gk.1 by Associate II
  • 3019 Views
  • 3 replies
  • 0 kudos

STM32WL55CCU6 : how to receive Uart1 data

Hi I am testing STM32WL55.I am testing UART1 of STM32WL55 by referring to SubGHz_Phy_PingPong​I can transmit data using UTIL_ADV_TRACE_Send.​I tried to receive data from terminal using UART1.But it didnot work.​I inserted UTIL_ADV_TRACE_StartRxProces...

Resolved! PM0271, Rev 3, errata and formula?

Hello ST - would you please clarify these two errata and share the missing formula from PM0271:Slot guard time (1.25 ms or 1.5 ms?The last sentence of 5.2 specifies a 1.25 ms guard time.5.2.2 specifies a 1.5 ms guard time and Figure 22 shows 1.5 ms g...

STM32WB BLE Beacon scanner

I want to use an STM32WB module as a ble beacon receiver/detector so I can monitor beacons on my PC using a uart or USB vcom? Are there any examples that can help me and if "Yes" where can I find them?

Is there a really simple STM32WB example?

All examples of the github repo are at least a few 10 of thousands lines of code big.I just want to share a few bytes of information over ble. Is there a really simple example without timeserver, freertos and that kind of stuff?Just like:start CPU2in...

NHand by Associate II
  • 1046 Views
  • 0 replies
  • 0 kudos

Resolved! SRAM2a retention in Standby not working on STM32WB55

Hi,I'm trying to make SRAM2a retention in standby mode work on my STM32WB55 device.As far as I can tell, the device enters and gets out of Standby as expected (the C1SBF and C2SBF flags are appropriately set when the MCU get sout of the low power st...

NSAUG.1 by Associate III
  • 2817 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.