STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

STM32WL with the LoRaWAN and the Sigfox coexistence

Hello, I would like to use the NUCLEO-WL with Sigfox and LoRaWAN in the code as proposed in the workshop (youtube video : MOOC - STM32WL workshop - 6 LoRaWAN and Sigfox coexistence). However, the zip project is not part of CubeWL. Thus, How can we up...

LLr.1 by Senior
  • 887 Views
  • 0 replies
  • 1 kudos

IEEE 802.15.4 BEACON Mode

Hello ST Community​,​I want to know if the STM32WB55RG supports MAC 802.15.4 Beacon Mode.​For now, I'm sure that the CM0+ Stack supports Only the Non Beacon Mode (SO=BO=15) and Full broadcast Mode (PANID 0xFFFF​, dest @ 0xFFFF) and OFC doesn't suppor...

MYous.3 by Associate II
  • 1296 Views
  • 1 replies
  • 0 kudos

LORA ping pong, point to point application

Hi all,I'am working with LORA and LORA-E5 chip, I'am trying to adapt the ping pong stm32 example (without lorawan). But for now I have a question, I'd like to have a point to point application, but my question is can I set a server and a client addre...

SBaro.11 by Associate III
  • 2350 Views
  • 4 replies
  • 0 kudos

Zigbee_DoorLock_Server_Coord Application in DEBUG mode

Hi,I try to launch the demo application called Zigbee_DoorLock_Server_Coord on a nucleo board WB55 with GDB and I have an error "Error on final launch" Device Debug Script (cf image)Others applications are OK.The application can run without GDB (RUN ...

Anto by Associate
  • 2023 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.