NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I am working on a lorawan-based project. I use STM32WB55. I know there are 2 cores in this MCU and ble is running on the second core. My code and other peripherals run smoothly when BLE thread is not running, But when the BLE thread is running...
I am using the Nucelo board and communicating with an IKS02A1 trough I2C2 using PINs PA11 and PA12 with the following configuration: I have initializaed the I2C folowing the guidelines in "stm32wlxx_hal_i2c.c", and when I use "HAL_I2C_IsDeviceReady()...
Hello guys, how are you?I'm investigating some .bss overflows i'm facing and i ended up on some weird question. Linker file for STM32WB generated by CubeMX is as follows:RAM1 (xrw) : ORIGIN = 0x20000008, LENGTH = 0x2FFF8RAM_SHARED (x...
Hi, do the STM32WB support Bluetooth 5.2 LE isochronous channels?Thanks!
Hello guys,I've been researching over the internet and in this forum about creating a composite device on STM32WB5M. I need to create a device that has a HID and a mass storage over the same USB. I saw some old posts saying it was not possible but at...
I'm designing a power line for the STM32WB55 microcontroller.I'm checking the power system on the Nucleo-68 board but I found that the microcontroller cannot send a Bluetooth signal if I connect Vsmps only when booting the microcontroller.I also foun...
My I2C doesn;t seem to work whenever i turn off debug pins in IOC. I used a diff to see the changes but it seems fine to my untrained eyes:$ git diff diff --git a/Core/Inc/sys_conf.h b/Core/Inc/sys_conf.h index 988f1e8..b3cb386 100644 --- a/Core/Inc/...
Hello,I am trying to use the LPTIM1 as a timeout counter of 5s. Each timeout the device would read a measured value from a sensor and send it by uplink.I want to trigger the LPTIM1 by software, but I do not know how to do this. This is probably a new...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.