STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

no radio Rx timeout after Radio.Rx() called

Hi,I use STM32WLE5CBU6. I created SubGHz Phy project. Device entered stop 2 mode, exit stop 2 mode when the alarm B interrupt issue then the Radio.Rx(3000) is called to receive data.my RTC Alarm interrupt function below,void HAL_RTCEx_AlarmBEventCall...

Hi, I'm trying to understand how storing and restoring the LoRa context for stm32wl works. To my understanding it would be ossible to skip the join process if the device is already joined once even if it is power cycled?

I've made sure "force rejoins at reboot" is not not ticked in the configuration file, and then I set the task "LoRaStoreContextEvent" in the beginning of the user code section like thisstatic void OnNvmDataChange(LmHandlerNvmContextStates_t state) {...

ABläs.1 by Associate II
  • 2268 Views
  • 2 replies
  • 0 kudos

STM32 WB BLE event handling

I put a debug message at the beginning of my event handler but the only event value I see is 0xFF. hci_event_pckt *event_pckt;evt_blecore_aci *blecore_evt;event_pckt = (hci_event_pckt *)(((hci_uart_pckt*)Event)->data);BLE_DBG_EEG_MSG("EEG Event %d re...

EHD by Associate II
  • 1634 Views
  • 1 replies
  • 0 kudos

Resolved! [STM32WB55] How to use CHAR_PROP_WRITE modified in sample code

Hi Sir,​I use sample code in STM32Cube_FW_WB_V1.13.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pServer and BLE_p2pClient. The BLE characteristic's property CHAR_PROP_WRITE_WITHOUT_RESP is used in the sample, I try to modified it as CHAR_PR...

LChan.5 by Associate II
  • 1648 Views
  • 1 replies
  • 0 kudos

About lora repeater

Can i use any stm32 mcu chip which used as lora repeater?Because i need in my project.Also give source code if available.

PPraj.1 by Associate II
  • 1393 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.