STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

LoRa Option in STM32 Cube for bl072cz-lrwan1

Hi I am trying to create SubGHz project using STM32 Cube. When I choose the bl072cz-lrwan1 board, although this is an eval kit for LoRa, and has a PingPong example which uses LoRa and SubGHz, yet I can't find any option for SubGHz or LoRa in the midd...

sgabran_0-1688681447642.png
sgabran by Associate III
  • 2828 Views
  • 3 replies
  • 0 kudos

Resolved! RSSI on LoRa module

HiWe are using the the ST library calculates LoRa SNR and RSSI by capturing the readings in register "REG_LR_PKTRSSIVALUE" although there is another register called "REG_LR_RSSIVALUE".I failed to figure out the difference in contents of those 2 regis...

sgabran by Associate III
  • 3092 Views
  • 1 replies
  • 2 kudos

PingPong Example, failing to run GPIO ISR

Hi I have been trying to activate the callback function for the pushbutton in the SubGHz PingPong example, but with no luck. I am using the BSP_PB_Init() to configure the pushbutton: void BSP_PB_Init(Button_TypeDef Button, ButtonMode_TypeDef ButtonMo...

sgabran by Associate III
  • 4321 Views
  • 6 replies
  • 1 kudos

LoraWan confirmed downlinks

Hello,I am trying to build an application on a STM32WLE5JBI6 that could work with confirmed downlinks. I thought that the LoRaMAC handled this but I could not find any mention of it in the documentation or in the code.As anyone already implemented it...

BLE air packet capture in STM32WB series

 I want to capture the BLE air packet to parse the BLE connection event by using nRF52840 Dongle and wireshark, but I met a problem.I can capture the air packet normally when the slave device is advertising. But once the connection is established, I ...

veryneo by Associate II
  • 1673 Views
  • 1 replies
  • 0 kudos

B-L072Z-LRWAN1 ERROR dev_nonce_too_small

Dear ST Community, Dear ST Team.For a evaluation of the chip i would like to try over LoRaWAN Communtication to set a LED on and off.Sadly on the  tutorial program LoRaWAN_End_Node i get the ERROR: dev_nonce_too_small. The Problem is that on the Docu...

RSheetz by Associate II
  • 1350 Views
  • 1 replies
  • 0 kudos

NUCLEO WB55RG both server and client

Hi, I am currently working on the NUCLEO WB55RG board on a project configured by CubeMX as BLE server. Everything is working correctly on this side. The problem is that I am using 4 boards as server and i would like to send a broadcast message (adver...

BasileC by Associate
  • 1138 Views
  • 0 replies
  • 0 kudos

Tickless idle on STM32WB55

I'm working on inserting the STM32WB55 into stop mode2 via the tickless idle for the FreeRTOSI saw that the SDK has an example for it: in the BLE_HeartRateFreeRTOS example for the nocleo wb55 I went over the code of the SDK and there was one line whi...

hagaimoshe_0-1688301926799.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.