STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

PLACE_IN_SECTION(..) macro linking issues

Throughout the codebase the PLACE_IN_SECTION macro is used to place bluetooth related static variables into their own sections. I guess this is done increase the isolation from possible errors in other parts of the code.The sections (for example "BLE...

HRadt.1 by Senior
  • 1778 Views
  • 1 replies
  • 0 kudos

STM32WB15 / 55 soil moisture sensor

Hi,I plan to design and build a soil moisture sensor for our plants at home, based on the STM32WB55 (I need ZigBee / Thread). But I want to build up a prototype by using my STM32WB15 nucleo board and some of these cheap Arduino Soul Moisture PCBs wit...

Kampi_0-1695368234340.png
Kampi by Associate III
  • 2224 Views
  • 0 replies
  • 0 kudos

Testing RTC_SSRU

I'm looking to create a test case to verify that the handling of the interrupt generated by RTC SSRU is working correctly.In the LoRaWAN code base, the SSR time is set up such that the underflow will happen after about 48.5 days.There doesn't seem to...

How do characteristics numbered and why do i get a gatt error

So I just don't get something in BLE,My service discovery says it is from 0x000C up to 0x0011. my service has 2 characteristics.but then I scan the characteristics in that range (from 000C to 0011 ) and get them but also get an gatt error on attribut...

Ebin34 by Associate II
  • 942 Views
  • 0 replies
  • 0 kudos

CE declaration of conformity for P-NUCLEO-WB55

Hello, I'm looking for the declaration of conformity document for the P-NUCLEO-WB55 pack [MCU STM32WB55RG (Nucleo68) and MCU STM32WB55CG (USB Dongle)]The document I need should reference the RF standards that the product is in compliance with.I check...

AMohe.1 by Associate II
  • 1060 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.