2024-03-01 3:25 AM - last edited on 2024-03-01 3:53 AM by Peter BENSCH
Good morning,
I am building a system with stm32 wl55jc1 to count water flow with a pulse flow meter.
So I created two internal clocks in stm32 one to create a time window and the other that counts each pulse received from the sensor. At the trigger of the first clock I check how many pulses the second clock counted and get the instantaneous flow rate.
I put an LED in parallel with the signal to visually see the pulses.
The problem is that the count the clock makes and the pulses I see do not match.
I would like to ask for some documentation on the input voltage and so that I can design my RC circuit as best I can (as I am convinced that the problem is electrical).
thanks for your time,
greetings
Roberto
Solved! Go to Solution.
2024-03-04 12:56 AM
Hello,
I solved it by inserting a clock filter, now it is very accurate.
Thanks anyway for the support.
Roberto
2024-03-03 5:16 AM
> The problem is that the count the clock makes and the pulses I see do not match.
What pulses do you see? What do you expect?
> I would like to ask for some documentation on the input voltage and so that I can design my RC circuit as best I can (as I am convinced that the problem is electrical).
The digital voltage thresholds are listed in the reference manual. Generally, the thresholds are around 0.3 * VDD and 0.7 * VDD.
2024-03-04 12:56 AM
Hello,
I solved it by inserting a clock filter, now it is very accurate.
Thanks anyway for the support.
Roberto
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.