STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Programming the STM32WB with Openocd

Hi,I need to program an STM32WB from a Raspberry Pi from the command line, preferably Python. I have got it up and running with my STM32FG0 but having no luck with the WB. From my understanding I need to:Program BLE Stack using FUS (Not sure how to d...

mrchips by Associate II
  • 4996 Views
  • 4 replies
  • 0 kudos

Resolved! LoRaWAN Project using P-Nucleo-LRWAN2

I am using P-NUCLEO-LRWAN2 package, and Nucleo STM32 L476RG as my end node.The end node is configured as :Region and Frequency plan: EU863-870Data is transmitted at: TX on freq 868100000 Hz at DR 0, TX on freq 868500000 Hz at DR 0, TX on freq 8683000...

NZama.1 by Associate III
  • 4674 Views
  • 3 replies
  • 1 kudos

Resolved! NUCLEO-WB09KE and STM32CubeMX generating wrong HAL files

Hi,I just try to get a NUCLEO-WB09KE board running.Unfortunately CubeMX (6.12.0) generates HAL files with a pattern of stm32wb0x_hal...,h but the include paths are stm32wb00x_hal (one more zero!)...Also in CubeIDE EXTI_HandleTypeDef is not found when...

AWack by Senior
  • 2280 Views
  • 4 replies
  • 1 kudos

STM32WB09KE VCAP Pin

Hi everyone,we are currently in the design phase with a STM32WB09KE Controller.Since we are designing the Power pins we have a question regarding the MLDO Vcap Pin.On the Nucleo Board there is a Cap placed with a value of 0.22uF where does this value...

Resolved! STM32WL End Node Example Project

Hi everyone,I'm new to working with STM32, and I've been using a custom board designed with the STM32C0 MCU to work with various peripherals. Now, I'm looking to create custom LoRaWAN sensor nodes that can measure data from sensors using ADC and tran...

nayeemcron_0-1725331107645.png

Resolved! STM32WB and Power control (Run and STOP0 mode)

Hi,I am working on the STM32WB55 with FreeRTOS and using the BLE stack on CPU2. Now, I need to implement STOP mode for the entire MCU. Ideally, I would like to put CPU1 into either RUN or STOP0 mode. I am used to handling this on simpler MCUs like th...

JR2963 by Senior II
  • 1611 Views
  • 1 replies
  • 1 kudos

Resolved! STM32WB05xN to replace BlueNRG-LPS

We planed the BlueNRG-LPS in one of our projects to use it as a Network Co-Processor via the ACI command set and also have some code ready for that. Can we now just switch it against an STM32WB05xN and use the same commands, or is their command set d...

OliM by Senior II
  • 2405 Views
  • 3 replies
  • 2 kudos

BLE Server and Router

I have been working with stm32wb5mm- dk and these need to be configured as router and server . I followed the examples P2P server and P2P Router  fromen.stm32cubewb-v1-20-0\STM32Cube_FW_WB_V1.20.0\Projects\P-NUCLEO-WB55.Nucleo.I used a very old smart...

Rituraj by Senior
  • 1453 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.