STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How to call Random Static Address in the past

Hello, I am developing a BLE HID device using the STM32WB55.I am generating random static addresses using a program implemented in the STM32CubeWB. This is used to identify multiple peripherals with the same functionality. #else /* Get RNG semaphor...

ELEHM by Associate II
  • 2643 Views
  • 4 replies
  • 1 kudos

Resolved! Is it possible to guide the HSE clock to MCO pin?

Hi,I would like to use the STM32WBA55 controller and forward the clock of the HSE to the MCO pin. The data sheet states that this is only possible for internal clocks:Clock-out capability:– MCO (microcontroller clock output): outputs one of the inter...

ledi7 by Associate III
  • 2154 Views
  • 2 replies
  • 5 kudos

Resolved! STM32WB55 AES2 bus faults when bonded over BLE

We are working on a product on the STM32WB55 that is hard faulting when trying to modify AES2 peripheral registers while actively bonded to a Windows PC over BLE.What we discovered is that we can use AES2 to encrypt and decrypt just fine, but the mom...

CMWX1ZZABZ (STM32L0) external reset issue

Hello,I have a custom board, equiped with a Murata CMWX1ZZABZ, running a firmware based on the LoRa and SigFox libraries provided by ST. Several hundreds, if not thousand, units are currently depoyed. For the most part, everything is fine.See the att...

VinceWnt by Associate
  • 1408 Views
  • 1 replies
  • 0 kudos

Resolved! Where can i find Hands-on_WS_WBA55.ioc file?

Hello,i want to start a Project based on Hands-on_WS_WBA55.ioc file, as descriped in STM32WBA5x Workshop - 4.But i only find on github the Hands-on_WS_WBA52.ioc file.Where can i download the file Hands-on_WS_WBA55.ioc?  

ledi7 by Associate III
  • 1490 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55CG Zigbee connection Tuya Smartlife with ST Example

Hi together,I have the STM32WB55CG on a custom PCB and plan to integrate it into a smart home Zigbee network, that uses a Tuya Gateway and is controlled by Smartlife app. I tried to use the project Zigbee_Find_Bind_OnOff_Router1 from the ST examples ...

vh789 by Associate III
  • 1771 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.