STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

I2C device detection issue

Hello ST Community,I recently encountered an issue that I have not come across before and am hoping someone can offer some insights.I have a custom board based on the STM32WB microcontroller, where I am trying to connect an I2C device. The board is a...

smirzaee by Associate
  • 2796 Views
  • 3 replies
  • 2 kudos

STM32WB with QSPI flash MT25QL256ABA (PMod SF3)

Hello all, I have a very strange issue with QSPI peripheral. I am using it to store logs in external memory. The flash that is used is MT25QL256ABA with a custom STM32WB55 board. I have connected PModSF3 using jumper wires that are at least 15cm long...

NRedd2_1-1729016790809.png NRedd2_0-1729016599271.png
NRedd.2 by Senior
  • 9993 Views
  • 11 replies
  • 0 kudos

P-Nucleo-WB55 Client Server use in parallel

Hello community,My problem generally consists of connecting and reading a BLE device into a BLE mesh network.The BLE device is a B-WB1M-WPAN1, from which I want to receive temperature data. I have written my own service and characteristisk for the te...

NUCLEO-WL55JC2 LPUART Not Working

Hey guys, I have NUCLEO-WL55JC2 board, and I am following a tutorial to learn baremetal embedded programming. The first task is a "hello world" app for UART. So, I just read the doc, and I understood that I need to use LPUART1 which is the default fo...

unalf by Associate
  • 1164 Views
  • 1 replies
  • 1 kudos

Resolved! stm32wb55 p2prouter and service

We are developing a Bluetooth application using the STM32WB55RG. According to the documentation, I found that using the Router and service approach can achieve a one-to-many connection. I want to know if, once a peripheral establishes a connection wi...

企业微信截图_20241030104206.png
CHEN25 by Associate II
  • 2967 Views
  • 6 replies
  • 0 kudos

I-CUBE-LRWAN

HiI'm working on a project where I have to take the humidity and temperature measures of the soil, and send them to a LoraWAN getaway. The problem is that I have to use the STM32L010F4P6 microcontroller and the RF module LAMBDA62C-9S. My question is ...

JCoo_15 by Associate
  • 1369 Views
  • 1 replies
  • 0 kudos

Resolved! How to export example projects from a STM32-FW-Package?

Hello, I am using CubeIDE v1.16.1 and I want to export a modified project from the firmware package STM32Cube_FW_WBA_V1.4.1. I modified the project directly in the corresponding example folder and it works successfully. Then I wanted to export the pr...

ledi001 by Senior
  • 2202 Views
  • 3 replies
  • 2 kudos

Current consumption numbers - TCXO included\not included

Hi,I have several questions regarding current consumption numbers as they appear in the Datasheet of the STM32WLE5.in Table 28 / Table 29 the current consumption of LORA RX/TX modes is mentioned.I have several questions:1. is it possible to use a TCX...

viola by Associate III
  • 2740 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.