STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How to put Matter Device into Sleep Mode

We are developing a Matter device using X-CUBE-MATTER.When we set CFG_FULL_LOW_POWER to 1 to enable sleep mode, pressing B1 for 10 seconds does not enter Factory Reset and BLE advertising is not executed.When we checked the current consumption, it se...

How to Write Correct Sleep Function for WB55?

I want to write a function for the STM32WB55 where BLE advertising is always active, and the processor performs the necessary tasks, then sleeps and wakes up using RTC Wakeup.I want to do it with STOP2 mode, but my processor consumes 3mA and does not...

Ygt by Associate II
  • 1672 Views
  • 2 replies
  • 1 kudos

Resolved! SWD and BOOT Pin lockout - STM32WL33

Hello,I am looking to add an STDC14 header to my design.I am concerned that by putting such a connector on the board, this will allow 3rd parties to simply buy an STLINK and reprogram my device.I am not familiar with STM32, so in the interest of spee...

CEagl.1 by Associate III
  • 1197 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLE5JC Adaptive Data Rate Implementation

Hi,I'm working with the STM32WLE5JC mcu and Cube firmware 1.13.0. Can someone explain how the module/stack implements adaptive data rate? I can see from lora_app.h that it is enabled by default, but exactly how is it implemented?The screenshot is fro...

helixembedded_0-1732033699454.png

LoRaWAN End Node JOIN FAILED

Hi community,I am using the STM32WLE5CC MCU on a self designed board and I am having problems to Join the device to my hub.The code is based on the LoRaWAN_End_Node example supplied by ST and addapted to my MCU following https://community.st.com/t5/t...

alefarri_0-1732727906118.png
alefarri by Associate II
  • 1038 Views
  • 1 replies
  • 0 kudos

Resolved! STM32wb55 Zigbee Network connection status

I'm trying to find a way to get the connection status of the Zigbee Network.Our application can successfully join a network. We have also implemented persistence and are able to rejoin a previously setup Zigbee Coordinator. But I haven't found a way ...

Oswalt by Associate
  • 4061 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.