NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi everyone,I am using the LoRaWAN_AT_Slave example code on an STM32WL-based device, and I am operating in OTAA mode with the ChirpStack server to monitor the data. I am successfully sending sensor data to the server at the specified intervals.I have...
Hello, I am planning to develop a 915 MHz LoRaWAN end node using the STM32WLE5C8U6. My goal is to send data from several sensors—such as GNSS, temperature, and accelerometer—directly to a gateway without employing an external MCU. 1- Could you please...
Hello,I would like to use the BLE_p2pServer_ota example with the STM32WBA55CG as a template for a project. Since I do not have an LSE available here, I would like to use the LSI. Which settings (defines) do I have to change?If I use the LSI with 32,0...
Hi, I'm testing a custom STM32WB09TEF7TR board. To communicate with the analog front end, I need to use SPI.However, SPI communication requires 17 us setting time, which means around 60 kHz.This speed is very slow.So, the Initiation of SPI becomes th...
Context:I have succesfully implemented a CDC device in a stm32f205 board 6 months ago.Now im trying to implement the exact same thing in my STM32WB5M discovery board.BLE is already activated and working P2P custom serverUsing CUBEMX 6.3.0FW package S...
Matter software expansion for STM32Cube v1.1.1. When I build 2_Images_SECoreBin on macOS development environment, the build fails probably due to postbuild.sh and prebuild.sh.Please let me know how to fix this.
we are working on STM32WLE5 development.We succeeded to enter Shutdown mode and measured supply current of less then 40nA when operated at 3.0V,but at that time, the VDDRF and VDDPA were not connected (0 volts), meaning we could not test the LoraWan ...
I'm trying to get a window cover to work, but can't seem to get the communication between attributes to work. I've been able to do this with the on/off cluster but this just doesn't seem to work. Also the examples on github are programmed very differ...
I want to add I2C support to a BLE sample project, in particular BLE_Beacon or BLE_Peripheral_Lite.In CubeMX on non-BLE projects I can select PB6-PB7 for SCL-SDA respectively.In a BLE project there is a clash with TIMER and the I2C code is not genera...
I have been using Seeed-LoRa-E5 github repository for my project. I have added code to send I2C sensor data to the LNS and the device joins and sends data successfully and the code works fine as expected. Now I want to add a timer interrupt and so I ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.