NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Using STM32CubeIDE 1.17.0, STM32CubeMX 6.13.0, MCU is STM32WB09KEV6TR.ioc file attachedHello,I am trying to write code for a PCB with an STM32WB09KEV6TR. I am very new to STM development. Before going any further in our project, I am simply trying to...
Hi,i am using the BLE_p2pServer_ota example with NUCLEOWBA55 and i want transmitt a 20 Byte package over USART2 with DMA in circular mode (19200 Baud). Here as an example, i send 20 bytes every second via HTerm to USART2. BLE advertising (every 2s) i...
I am working on a low power mode in a freeRTOS ble application. On a user request the device is to go into low power mode Stop2. In order to achieve the lowest power consumption ~2µA (stm32wb55) the ble activity has to be deactivated and the cpu1 & c...
Moved from MPUs forum.Hi, I looking to use the Nucleo WB55RG board to prototype some BLE firmware.I was looking through the examples in Cube MX but that particular board wasn't listed but there were a few similar choices, (see below). I was thinking ...
I am working with STM32WB55RG microcontroller. The application that I am working on needs to enter BLE mode when requested by user. I am able to start the BLE application and it starts advertising.After a set time of 1 minute the application has to c...
Hi,When the device is first added to Apple HomePod, pressing button 2 can trigger automation, and it is always effective no matter how many times it is triggered. But once the device restarts, pressing button 2 again is almost always ineffective. Gue...
Hello,I'm using the B-WL5M-SUB1G, using Visual Studio as my programming environment, attempting to get LoRa TX working without using the middleware.The code is below. The project serial output is below the code block. Referencing RM0453 Rev 6 (STM32W...
Hi,I have the problem, that my MCU seems to loose its connection to the network quite often (after some minutes or hours usually) and is therefore not usuable.I would like to detect this in my Application and then trigger either a rejoin (if possible...
Hello, I have an STM32WB55 processor. I use BLE. I use FreeRTOS.I call the functions HAL_PWREx_EnterSTOP1Mode or HAL_PWR_EnterSLEEPMode.Before that I call the HAL_SuspendTick function.But somehow I exit WFI. Somehow an interrupt comes but I couldn't ...
Hi, I'm using the LoRaWAN end node example from the stm32cubewl v1.3.0. The board im using is the RAK3172 based on the stm32wle5ccu6 chip. The application i want to build reads data from a modbus using UART and sends it through lorawan. I have assign...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.