STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB55REVx Custom board Schematic Review

I am working on a new project which is based on STM32WB55REVx MCU. I have designed the schematic as shown based on the VDD 1.8V. I would like to understand whether the power lines and RF design is properly done, or it needs some changes. I would appr...

STM32WB55REVx Schematic.png
Sangratha by Associate II
  • 2924 Views
  • 8 replies
  • 1 kudos

Address for DEVEUI,JOINEUI and APPKEY

Hi,In RAK3172 which have STM32WLE5CCU6, during the flashing of DEVEUI,JOINEUI ,APPKEY and NWKKEY in which memory location of NVM this values are being stored. Is there any documentation for same? Also can we flash these keys directly to NVM using STM...

pho3nix by Associate III
  • 1616 Views
  • 1 replies
  • 0 kudos

Resolved! Connection with Garmin devices with privacy enabled

Our product is based on an STM32WB5MM. On the STM32WB, we have privacy enabled and use the filter/acceptance list.When the filter/acceptance list is not enabled, we want the device to be able to connect to a Garmin device. Unfortunately, the device d...

Resolved! STBLEToolbox not discovering devices

I have a HC-06 module being run via USART from a STM32F411RE NUCLEO board.When I run STBLEToolbox (or LightBlue) the module doesn't appear in the scan list (all filters are off)Yet when I open my Bluetooth settings on my phone the module shows up & I...

Resolved! STM32WL33: send the raw HF Data to a GPIO Pin

Hi everyone,I'm at the start to build up my transceiver based on the STM32WL33 with the Nucleo-board NUCLEO-WL33CC1 and the Mainboard MB1801. I want to use the IOC in the Cube IDE.If you are trying to send the raw HF Data to a GPIO Pin:  Change  __HA...

BLE receive data DMA and TASK Sequencer

Hello, I am making BLE data logging application where STM32WB35 series working as peripheral and sending to laptop the sensor data every second. STM32WB35 is receiving data from sensor on UART and sending same data to laptop every second on BLE. The ...

Nico3 by Senior
  • 1091 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.