STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Compilation Warning in STM32_WPAN package

Hi, I'm working with STM32_WPAN package (attached), on STM32CubeIDE (gcc compiler). MCU: STM32WB55 There's a Compilation Warning that I don't know how to deal: converting a packed 'TL_EvtPacket_t' pointer (alignment 1) to a 'tListNode' {aka 'struct _...

AFink_0-1706515676051.png AFink_0-1706516168038.png
AFink by Associate III
  • 2563 Views
  • 3 replies
  • 1 kudos

Scan result BLE stm32 observer

Hello,I have changed the program based on p2p_client, app_ble.c to a program in which it is only an OBSERVER or BEACON SCANNER Until now I have been able to run the scan function but I don't know how to get or display what device I am scanning.I have...

Aboyh_0-1740124150801.png Aboyh_1-1740124662816.png
Aboyh by Associate II
  • 1026 Views
  • 2 replies
  • 0 kudos

STM32WB5MMG SPI not working

Hi, I made a custom board with the STM32WB5MMG module. The custom board contains just the STM32WB5MMG module with pins connected to some of the GPIOs of the module.  I tried to interface this custom board with AD5940 potentiostat via SPI in order to ...

Screenshot 2025-04-02 153046.png Screenshot 2025-04-02 155407.png Screenshot 2025-04-02 194235.png sam111_0-1743640971753.png
sam111 by Associate II
  • 974 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL UART bootloader

Hi all, Just a question, I have one stm32wl RAK3172 chip, on this chip I have a stm32f4 connected via UART like thatSTM32F4 UART2             RAK3172 UART1 PD6               ---->            PB6.   PD5              ----->           PB7   I'm trying t...

SBaro.11 by Associate III
  • 1377 Views
  • 1 replies
  • 0 kudos

Thread time sync using WB55

Hello all,   I am trying to use the time sync service from openThread, using a P-NUCLEO-WB55. For that purpose, I am using the sample Thread_FTD_Coap_Multicast that is working properly. I am using the latest stm32wb5x_Thread_FTD_fw.bin image for the ...

STM32WLE5CCU7 I2C Not Working

Hi,Currently, we are working on the IO-EXPANDER (PCA9505DGGY) via I2C communication. We are using Standard mode (100 kHz).Whenever we try to communicate with the slave device, the SDA line remains idle, and I can only see three clock pulses on the SC...

BLE Client program on Nucleo WB55RG

Hi Team,  We are using Nucleo W55RG board for testing BLE.  We have a requirement to configure the Nucleo board as Client ( Able to connect to an advertising device) and able to send data to an external Advertising device.  We are trying to explore t...

Tej by Associate
  • 1022 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.