2025-03-31 6:44 AM
Hi,
I'm relatively new with ST microcontrollers and I'm struggling a bit to find an answer to a question I have.
I have some code that reads data from an external source. I need to read some data on startup, as it dictates the some stages of the boot process. The code that parses that received data also sends notifications over BLE later in the program execution. My problem is that the first calls to my parser triggers some notifications before the BLE interface is properly initialise and the micro hard-faults.
I can't bring the call to `app_BLE_init()` any earlier than it is. I was wondering if there's a function in the API to check the status of the BLE stack, and avoid acting on the BLE link before it has been properly initialised. I tried with a dirty boolean flag, but I'm sure there must be a better way, right?
Solved! Go to Solution.
2025-04-10 2:01 AM
In case someboyd finds this, I ended up setting a flag on the "SHCI_SUB_EVT_CODE_READY" event:
// in app_entry.c
static void APPE_SysUserEvtRx(void * pPayload)
{
[...]
switch (p_sys_event->subevtcode)
{
case SHCI_SUB_EVT_CODE_READY:
[...]
osEventFlagsSet(SystemFlags, SF_BLE_INITIALISED);
break;
[...]And then I used this function as my check
bool isBLEReady(void)
{
return osEventFlagsGet(SystemFlags) & SF_BLE_INITIALISED;
}
2025-04-10 2:01 AM
In case someboyd finds this, I ended up setting a flag on the "SHCI_SUB_EVT_CODE_READY" event:
// in app_entry.c
static void APPE_SysUserEvtRx(void * pPayload)
{
[...]
switch (p_sys_event->subevtcode)
{
case SHCI_SUB_EVT_CODE_READY:
[...]
osEventFlagsSet(SystemFlags, SF_BLE_INITIALISED);
break;
[...]And then I used this function as my check
bool isBLEReady(void)
{
return osEventFlagsGet(SystemFlags) & SF_BLE_INITIALISED;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.