2025-09-23 11:35 AM
Dear Community,
I have the B-WBA5M-WPAN module and trying to get a basic OpenThread Project working with Demo Code provided.
The Demo Code provided for the module is not sufficient - I am trying to change LED Color when button B2 is pressed.
I am trying to copy code examples for the NUCLEO-WBA55CG, but it is not working as there any many dependencies in the BSP file unique to the NUCLEO Board.
I also can't find a proper Application Note for the module.
Any assistance will be greatly appreciated.
2025-09-24 12:42 PM
I found these macros:
#ifdef CFG_BSP_ON_DISCOVERY
#include "stm32wba55g_discovery.h"
#if (CFG_LCD_SUPPORTED == 1)
#include "stm32wba55g_discovery_lcd.h"
#include "stm32_lcd.h"
#endif /* (CFG_LCD_SUPPORTED == 1) */
#endif /* CFG_BSP_ON_DISCOVERY */
#ifdef CFG_BSP_ON_CEB
#include "b_wba5m_wpan.h"
#endif /* CFG_BSP_ON_CEB */
#ifdef CFG_BSP_ON_NUCLEO
#include "stm32wbaxx_nucleo.h"
#endif /* CFG_BSP_ON_CEB */It seems like CubeIDE is not enabling it for some reason - can anyone perhaps point me in the right direction to enable CubeIDE to select the correct macro?
2025-09-26 3:25 AM
Double checked and the flags are not the reason for code not being generated.
I am in the process of porting the code from the Nucleo Example to work on the WBA5M-WPAN, bypassing some of the BSP Function calls.
2025-09-29 12:15 PM
In STM32CubeIDE I chose the STM32WBA5MMG Processor instead of the B-WBA5M-WPAN - worked to some extent and generated missing code.
In CubeMX I enable CRC. Computing -> CRC.
It generates related files.
Once STM32WPAN is enabled, the CRC-related files go missing and I am left with this error:
I copied related files from the sample code, but then the error code states that crc.c and crc.h files are missing.
../Core/Src/app_entry.c:40:10: fatal error: crc_ctrl.h: No such file or directory2025-09-29 1:08 PM
I included related files from this link.
../Core/Src/crc_ctrl.c:26:10: fatal error: crc_ctrl_conf.h: No such file or directory
Still searching for the above files.
2025-10-07 4:28 AM
UPDATE:
Code Crashes on this line:
LinkLayerTaskHandle = osThreadNew(LinkLayer_Task_Entry, NULL, &LinkLayerTask_attributes);
LinkLayerTaskHandle returns nil.
This is part of ll_sys_if.c
This is the function:
void ll_sys_bg_process_init(void)
{
/* Create Link Layer FreeRTOS objects */
LinkLayerSemaphore = osSemaphoreNew(1U, 0U, &LinkLayerSemaphore_attributes);
LinkLayerTaskHandle = osThreadNew(LinkLayer_Task_Entry, NULL, &LinkLayerTask_attributes);
if ((LinkLayerTaskHandle == NULL) || (LinkLayerSemaphore == NULL))
{
LOG_ERROR_APP( "Link Layer FreeRTOS objects creation FAILED");
Error_Handler();
}
}
2025-10-07 4:30 AM
I believe this to be linked to the CRC function.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.