2019-07-11 11:04 AM
Hello,
I have a B-L072Z-LRWAN1 module and use AT commands, but I do not know how to change the frequency I need 915Mhz, but when I use the command AT + TCONF =? It shows me the following:
Freq = 868 MHz
Power = 14 dBm
Bandwidth = 125 kHz
SF = 12
CR = 4/8
LNA State = 0
PA Boost State = 0
868: 14: 125: 12: 4/8: 0: 0
then I change the compilation options, but there are no changes when executing this command, that is, the frequency always shows it in 868Mhz
2019-07-11 12:14 PM
Hard coded constant in
STM32CubeExpansion_LRWAN_V1.1.2\Projects\Multi\Applications\LoRa\AT_Slave\src\test_rf.c
static s_loraParameter_t loraParam= { F_868MHz, P_14dBm, BW_125kHz, SF_12, 4, 0, 0};
2019-07-11 12:27 PM
Thank Clive, now work fine:
AT+TCONF=?
Freq= 915 MHz
Power= 14 dBm
Bandwidth= 125 kHz
SF= 12
CR= 4/8
LNA State =0
PA Boost State =0
915:14:125:12:4/8:0:0
2019-07-11 12:34 PM
So, there are a documento where this level of setting is show?
Thanks
2019-07-11 6:00 PM
I just searched the source files with a file manager.
Looks to have been overlooked, probably needs to use the define set elsewhere for the frequency.
This bug has been there for a while, not seen any questions on the forum about it before.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.