cancel
Showing results for 
Search instead for 
Did you mean: 

Auracast with Galaxy S24 phone - only first channel or subgroup

Sandeep_k
Associate III

Hello,

Right now I am using 2 STM32WBA55G-DK1, one as PBP_Source and other is TMAP_Peripheral. The source consists of 2 BIS channels and in TMAP, I have included language selection option to include the subgroup or channel selection. And its working fine. But if I select Unicast option and pair with S24 mobile, only first channel or subgroup I can select, not the 2nd one. May I know whats the reason and how to overcome from this.

 

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
TPITEL
ST Employee

The 3.5mm jack used as an input for the Discovery kit can only carry 2 channels so you either have 1 stereo track or 2 mono tracks. It's not possible with this setup to get 2 stereo tracks.

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

You mean a Samsung Galaxy S24 phone?

What software version is it?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TPITEL
ST Employee

Hi Sandeep,

From what I understand, you are trying to use the Samsung Galaxy S24 as a Broadcast Assistant to synchronize the DK to your multi-language source. Can you confirm this ?

If yes, the reason you can only see one subgroup is that Samsung doesn't support synchronization to multi-language sources. To my knowledge it's not supported by any other smartphone. If you want to test a compatible Broadcast assistant, please check our implementation on STM32WBA: https://github.com/stm32-hotspot/STM32WBA-BLE-Audio-Broadcast-Assistant.

Regards,

Tom.

Sandeep_k
Associate III

Thank you for your kind response sir.

I have another doubt that after sending 2 songs and dividing them into 2 BIS, is it possible to get them as a stereo song in the receiver at the final stage?

If that's answered you question, please mark the solution.

For a new question, please start a new thread - you can always give a link back to this thread, for reference, if you want.

And give a link here to the new thread, so that people can find it.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Sir, is it possible to get the stereo audio in the below condition.

"I have another doubt that after sending 2 songs and dividing them into 2 BIS, is it possible to get them as a stereo song in the receiver at the final stage?"

 

Thank you

 

TPITEL
ST Employee

The 3.5mm jack used as an input for the Discovery kit can only carry 2 channels so you either have 1 stereo track or 2 mono tracks. It's not possible with this setup to get 2 stereo tracks.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.