2021-06-30 12:17 PM
2021-06-30 7:41 PM
I assume you mean a short between 3V3 and GND. I don't think anything would explain that behavior other than a solder bridge or similar between 3V3 and GND, especially if the chip isn't even powered. If you resolder it to the board, does the short come back or stay away?
2021-07-02 7:56 AM
Yes, short between 3V3 and GND. Batteries were connected after assembly, so there was current on 3V3 line. When chip was resoldered, the short went away on both board and chip.
2021-07-02 8:56 AM
> When chip was resoldered, the short went away on both board and chip.
I don't see what else would explain it other than a solder bridge. Given that the xray turned up 3 of them, seems plausible it may have missed some as well. Clearly there were manufacturing issues.
That's a cool xray reconstruction photo.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.