cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-TOUCHGFX 4.24.0 is out!

LouisB
ST Employee

TouchGFX 4.24.0 is now out.

Please follow this link to download it.

4.24.0 Release details:

  • Release date: June 6th, 2024

  • New TouchGFX Designer Features:

    • Added a QR Code widget.
    • Added RGB Compression for images.

  • New TouchGFX Core Features:

    •  Added RGB Image Compression for 16bpp, 24bpp and 32bpp framebuffer
      formats.
  • Bugfixes in TouchGFX Designer:

    • Fixed a bug where small screens were not able to display the language
      settings properly.
    • Fixed a bug where copying and pasting widgets from one screen to another
      would invert the order of the widgets.
    • Fixed a bug where a user was able to modify the canvas while being in a
      different tab, by copying and pasting widgets selected on the canvas.
    • Fixed a bug where the user was unable to edit the name of a widget with
      the F2 key while being placed inside a container.
    • Fixed TextureMapper not showing an image when copying and pasting a
      TextureMapper.
    • Fixed the text in Log View being editable.
    • Fixed erroneous default value behavior for Shade Alpha in ModalWindow.
    • Fixed toggling Framework features not signaling outdated code or unsaved
      changes.
    • Fixed a bug when importing custom containers where certain zipped
      archives would cause a crash.
    • Fixed changing simulator skin not showing outdated code or unsaved
      changes.

  • Bugfixes in TouchGFX Core:

    • Removed warning in image converter of unsupported 'viewBox' attribute in
      SVGs. For more information please read the article about SVG.
    • Vector fonts and SVGs now also work for rotated displays on GPU2D
      (NeoChrom) targets.
  • Bugfixes in TouchGFX Core:

    • Removed warning in image converter of unsupported 'viewBox' attribute in
      SVGs. For more information please read the article about SVG.
    • Vector fonts and SVGs now also work for rotated displays on GPU2D
      (NeoChrom) targets.
  • Deprecated TouchGFX Core Features:

    • Removed types from Types.hpp:
      • FrameBuffer::FB_PRIMARY
      • FrameBuffer::FB_SECONDARY
      • FrameBuffer::FB_TERTIARY
      • Gradient::GRADIENT_HORIZONTAL
      • Gradient::GRADIENT_VERTICAL

4.23.2 Release details:

  • Release date: March 14th, 2024

  • Bugfixes in TouchGFX Designer:

    • Fixed a bug where TouchGFX Designer would not close properly
  • Bugfixes in TouchGFX Core:

    • Fixed issue were accessing cached bitmap data could result in unaligned
      memory accesses.
  •  

Feel free to learn more about our new features by looking into our documentation !

Note : TouchGFX Designer 4.24.0 MUST be used with STM32CubeMX 6.11.0 or above (link to download STM32CubeMX).

Attention : If X-CUBE-TOUCHGFX 4.24.0 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-24-0.zip file to install the new pack inside STM32CubeMX.

 

Please also check our Known Issues article.

 

Enjoy this new version ! :)

Louis BOUDO
ST Software Engineer | TouchGFX
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0