2015-09-10 5:06 AM
Excuse my English, I am using Google translator.
I use STM32F7. I have two problems. 1) The colors of the camera are not displayed correctly, here are some photos of my problem: [[this link/image has been flagged as malicious by our security scan software and has been deleted]] 2) The display is updated slowly. But the picture is displayed quickly if it is one, and there is a delay: // ------ fast displayPosL1(320, 240, 0, 0); Camera_SnapshotStart(); HAL_Delay(200); displayBackgroundL1((uint32_t)&cameraImage); // ------ // ------ slowly: displayPosL1(320, 240, 0, 0); Camera_SnapshotStart(); HAL_Delay(100); displayBackgroundL1((uint32_t)&cameraImage); // ------ // slowly: while(1){ displayPosL1(320, 240, 0, 0); Camera_SnapshotStart(); HAL_Delay(100); displayBackgroundL1((uint32_t)&cameraImage); // Quickly the first time only HAL_Delay(1000); // ------ }; // ------ Videos: fast - slowly - #ltdc #stm32f7 #cacamera #ov76702015-09-10 1:05 PM
1) The colors of the camera are not displayed correctly, here are some photos of my problem:
Well, obviously the pixel format of camera as grabbed by mcu, and of the display controller, don't match... I am not going to guess, what's wrong. You should thoroughly study the available documentation for camera, the camera interface on mcu, and the lcd; and of course you shouldn't rely on some pre-baked software of dubious origin (''library''). You can also experiment: start with a single color (a piece of red paper, say), trying to match a single channel of the camera (i.e. ''as purely red as possible'', ''as purely green as possible'', ''as purely blue as possible''); change its intensity (change external illumination) and observe changes the obtained picture. If the camera has AGC or automatic color corrections, this may prove an impossible exercise. > 2) The display is updated slowly. > But the picture is displayed quickly if it is one, and there is a delay: Why do you believe it should be faster? JW PS. I don't know what is your mother tongue, but there might be helpful fora in your language out there - e.g. if you speak Russian, try caxapa.ru/arm.html2015-09-10 11:57 PM
1) Thanks, I'll try to deal with it
2) I found a solution to the problem, it was the fact that the camera is working at 7fps On the forums with my tongue no one helps :(We’re moving the ST Community to a new platform to give you a better and more reliable community experience.