2025-07-16 4:10 AM
I’m working on a TouchGFX project with a dropdown menu. When I select an option, the selected text is shown in a TextArea using a wildcard buffer (selectedTextBuffer).
In the TouchGFX Simulator, the full string displays correctly. But on the actual STM32 board, only the first letter (e.g., just "M") is visible.
I've already tried the following:
Set the buffer size in Designer to 32
Confirmed that all characters are included in the font's wildcard character set
Verified that invalidate() is called after updating text
Rebuilt assets and fully flashed the board
Despite all this, the board still only shows the first letter.
Setup:
MCU: STM32H7 (STM32H750-DK)
TouchGFX version: 4.25.0
TextArea uses selectedTextBuffer as wildcard
Solved! Go to Solution.
2025-07-23 12:18 PM
If you changed the text displayed to something else, "Test", does it always show only the first letter?
Yes
If you add more M's (keep them capitalized), will it display them?
No, only first letter
Are you using Typed text or creating the text programmatically with snprintf?
creating using snprintf
If you don't use a wildcard but simply place text in there will it display correctly?
Yes It does.
Anyways I used the textID of the buttons in the dropdown menu to set to my desired wildcard text. It worked for me.
Thanks!
2025-07-17 4:02 AM
Hello @BTKottary27,
Your text area is big enough to show all the characters ? Try to call resizeToCurrentText() TextArea | TouchGFX Documentation.
BR,
2025-07-17 5:17 AM
tried resizeToCurrentText() , No changes. It works perfectly fine for me in simulator but not on board!
2025-07-22 1:22 AM
Hello @BTKottary27
You can try to debug the target, check what value is passed to the textArea and if the invalidation is made correctly.
BR,
2025-07-23 7:59 AM
Were you able to resolve this?
If you changed the text displayed to something else, "Test", does it always show only the first letter? If you add more M's (keep them capitalized), will it display them? Are you using Typed text or creating the text programmatically with snprintf? If you don't use a wildcard but simply place text in there will it display correctly?
2025-07-23 12:18 PM
If you changed the text displayed to something else, "Test", does it always show only the first letter?
Yes
If you add more M's (keep them capitalized), will it display them?
No, only first letter
Are you using Typed text or creating the text programmatically with snprintf?
creating using snprintf
If you don't use a wildcard but simply place text in there will it display correctly?
Yes It does.
Anyways I used the textID of the buttons in the dropdown menu to set to my desired wildcard text. It worked for me.
Thanks!
2025-07-23 1:28 PM
Great! That's probably the better way to go as it supports localization (different languages, formatting).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.