2020-11-18 1:12 AM
Hello,
I used the SMT32F429i-DISC1 and TouchGFX follow the user guide
coding, why the touch point and the displayed position are exactly opposite?
For example, if my button is on the far left, I have to press the far right position of panel to respond?
Thanks
2021-08-11 1:25 AM
Which application template are you using from TouchGFX Designer?
2021-08-11 1:27 AM
I'll ask with the team responsible for ATs if they're aware of any current issues with the new 429-disc board.
2021-08-11 8:51 AM
Hello,
I got the blue board MB1075-F429I-E01
I used TouchGFXdesigner 4.14.0
I upgraded now to 4.16.1 , This version works now with my board, it has a different board selector and produces the right code.
The compiled binary firmware file from the board support page does not work with my board.
/Oliver
2021-08-12 3:15 AM
Thanks for the feedback, @OHenr.1
2022-02-23 6:13 AM
Hello guys,
Did you guys find a solution for this problem? I am using TouchGFX 4.18.1 and the displayed positions are still reversed.
Thank you!
2022-07-29 11:59 AM
Not sure if this helps anyone, but I had this issue when I choose the wrong stm32f429 variant.. D1 instead of E1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.