STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.

helloI want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.​An operation has occurred.​used STM32H735G-DK ​/ CubeIDE 08:16:59 : STM32CubeProgrammer API v2.9.0 08:17:02 : ST-LINK SN...

mSH.1 by Associate III
  • 1406 Views
  • 2 replies
  • 0 kudos

Resolved! An error occurs about the screen deleted from TouchGFX.

hello​An error occurs about the screen deleted from TouchGFX.​I deleted a specific screen from TouchGFX and re-generated the code.Also, CubeIDE also deleted the Cpp file corresponding to a specific sceen.​Then it builds normally.​However, the problem...

mSH.1 by Associate III
  • 1934 Views
  • 2 replies
  • 0 kudos

Resolved! Array of Widgets

To customize a TouchGFX application created with the TouchGFXDesigner, I am trying to create a screen with many circles that can be updated, for that I use an array to store the circles and the circles painters, but then when I try to access the meth...

JVALL.1 by Associate III
  • 1650 Views
  • 2 replies
  • 0 kudos

Resolved! Preloading a QSPI with STM32CubeIDE

I'm working on a project using an STM32H753XI MCU with a touch display. I am not currently using TouchGFX. I would like to preload images into the onboard QSPI during the project load. How do I go about doing this? I have used TouchGFX designer o...

RLein.1 by Associate III
  • 1800 Views
  • 2 replies
  • 0 kudos

STM32F413H-Discovery board issue about Touchscreen Calibration : ERROR (because of ts_status = TS_DEVICE_NOT_FOUND; )

Hi, MCD teams, I bought a new STM32F413H-Discovery board (MB1274-F413HT6-E03 A214500149) from Mouser and received it on last week.Now I tried to run the application under the folder of F4 Firmware Package\Demonstrations\STemWin\MDK-ARM\Project.uvproj...

Echan.1 by Associate II
  • 1870 Views
  • 2 replies
  • 0 kudos

Resolved! Does anyone have a working example of Partial frame strategy on a STM32f407 device with an FSMC linked screen controller like SSD1963?

I am trying to get basic TouchGFX graphics working on STM32F407 over FSMC to an SSD1963 screen controller. I am getting the following errors on compile:#error "a user must call touchgfx::startnewtransfer(); once touchgfxDisplayDriverTransmitBlock(): ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.