2019-01-03 1:16 AM
When will STM32CubeMX support STM32L4+ TouchGFX ? We have a project waiting for this.
2019-01-09 4:22 AM
Hi @MHo.15 ,
Did you tried using latest STM32CubeMX version (5.0.1)?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-01-10 1:08 AM
Hi Amel,
Yes, it's 5.0.1. The only available support is STemWin. TouchGFX option never shows up. Do you know what's wrong ? Or can you provide me an example CubeMX project with STM32L4+ and TouchGFX enabled ? Thanks a lot !
2019-01-15 11:12 AM
I have the same problem.
There is also no "ST-TouchGFX-x.x.x.msi" installer in the L4 firmware package. It would be good to know when TouchGFX support for L4/L4+ will be integrated into STM32CubeMX. It would be also nice to get directions on workaround for this issue until CubeMX and firmware packages will be updated.
Thanks.
2019-02-13 6:20 AM
Any News on this? L4/L4+ already supported by TouchGFX?
2019-03-01 3:07 AM
Any update on this ? Just tried CubeMX 5.1.0 and still no integrated support for L4+.
2019-05-13 7:22 AM
Hi Amel, is there any update on this issue ? Thanks.
2019-05-13 12:21 PM
Same question.
I have just updated STM32CubeMX to version 5.2.0 and even installed the new STM32CubeIDE v 1.0.0 (with CubeMX integrated).
None of them has TouchGFX support for STM32L4R (only STemWin can be enabled in "GRAPHICS").
Very disappointing.
2019-05-14 3:57 AM
Hi guys,
I'll try to get an update on this.
/Martin
2019-05-14 5:14 AM
Okay, seems STM32L4R will be supported with release 6.0 by the end of the year.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.