2025-01-06 12:03 AM - last edited on 2025-01-06 8:10 AM by GaetanGodart
In my main screen there is a scroll wheel which scrolls the contents of a custom container. The custom container has 5 wildcards. Now I intend to dynamically update those wildcards with my text resources. But I'm unable to do so. Please find my codes attached.
Screen1View.cpp
#include <gui/screen1_screen/Screen1View.hpp>
#include <texts/TextKeysAndLanguages.hpp>
void TextUpdate::updateText()
{
Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
textArea1.setWildcard(textArea1Buffer);
textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));
add(textArea1);
}
// Screen1View constructor
Screen1View::Screen1View()
: tickCounter(0), targetItem(0), scrollCompleted(false),
digitalHours(0), digitalMinutes(0), digitalSeconds(0),
textUpdateIntervalCounter(0), textUpdateObj() // Initialize textUpdateObj
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
tickCounter = 0; // Reset the tick counter
textUpdateIntervalCounter = 0; // Reset the interval counter
targetItem = scrollWheel1.getSelectedItem(); // Initialize target item
scrollCompleted = false; // Reset scroll completion flag
digitalHours = digitalClock1.getCurrentHour();
digitalMinutes = digitalClock1.getCurrentMinute();
digitalSeconds = digitalClock1.getCurrentSecond();
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::handleTickEvent()
{
tickCounter++;
textUpdateIntervalCounter++;
// Scroll logic: Execute every 0.5 seconds (30 ticks at 60 Hz)
if (tickCounter % ticksPerStep == 0)
{
if (!scrollWheel1.isAnimating() && !scrollCompleted)
{
targetItem = (targetItem + 1) % scrollWheel1.getNumberOfItems();
scrollWheel1.animateToItem(targetItem, 500); // Smooth animation (500ms)
scrollCompleted = true;
}
else if (!scrollWheel1.isAnimating() && scrollCompleted)
{
scrollCompleted = false; // Reset flag when animation finishes
}
}
// Clock update logic: Execute every second
if (tickCounter % 60 == 0)
{
textUpdateObj.updateText();
if (++digitalSeconds >= 60)
{
digitalSeconds = 0;
if (++digitalMinutes >= 60)
{
digitalMinutes = 0;
if (++digitalHours >= 24)
{
digitalHours = 0;
}
}
}
digitalClock1.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
}
// Text update logic: Execute every 2 seconds (120 ticks at 60 Hz)
if (textUpdateIntervalCounter >= 120)
{
textUpdateObj.updateText(); // Update text dynamically
textUpdateIntervalCounter = 0;
}
}
void Screen1View::resetScroll()
{
tickCounter = 0; // Reset tick counter
scrollCompleted = false; // Allow scrolling again
}
Screen1View.hpp
#ifndef SCREEN1VIEW_HPP
#define SCREEN1VIEW_HPP
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
#include <gui_generated/containers/CustomContainer1Base.hpp>
class TextUpdate : public CustomContainer1Base
{
public:
// TextUpdate();
//virtual ~TextUpdate(){}
virtual void updateText();
};
class Screen1View : public Screen1ViewBase
{
public:
Screen1View();
virtual ~Screen1View() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void handleTickEvent();
void resetScroll(); // Method to reset the scroll state
protected:
int tickCounter; // Counter to track ticks
int targetItem; // The target index for the scroll wheel
bool scrollCompleted; // Flag to ensure the scroll happens only once
static constexpr int ticksPerStep = 30; // Number of ticks for a 0.5-second delay (assuming 60 Hz)
int digitalHours;
int digitalMinutes;
int digitalSeconds;
int textUpdateIntervalCounter; // Counter for updating text every 2 seconds
TextUpdate textUpdateObj; // Object for TextUpdate
};
#endif // SCREEN1VIEW_HPP
I intend to print only in the first wildcard for the time being.
2025-01-06 12:42 AM
add(textArea1);This update text on other paralel universum... try
textArea1.invalidate();
2025-01-06 1:29 AM
I did try,
textArea1.invalidate();But it still does not update any wildcards
2025-01-06 3:18 AM
void TextUpdate::updateText()
{
Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
textArea1.setWildcard(textArea1Buffer);
textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));you update nothink then you nothink change see...
2025-01-06 3:25 AM
I have tried both these variations
void TextUpdate::updateText()
{
Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
textArea1.setWildcard(textArea1Buffer);
textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));
add(textArea1);
textArea1.invalidate();
}and
void TextUpdate::updateText()
{
Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
textArea1.setWildcard(textArea1Buffer);
textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));
textArea1.invalidate();
}
2025-01-06 3:40 AM
Have you basic C++ knowledge?? Your try work with containers is complete wrong.
2025-01-06 3:48 AM
Hi @Roombr_VI
Please share an example project with the code in your question.
2025-01-06 8:17 AM
Hello @Roombr_VI ,
Sharing your whole project (as a 7z file) would help us understand what you want to achieve.
The scrollWhell uses callbacks to update its elements (the custom containers that are inside the scrollWheel).
There are 2 native callbacks :
You read the API documentation for the scrollWheel here .
Also, to setup these callbacks, I invite you to watch this video (on 75% or 50% speed maybe).
Regards,
2025-01-07 1:30 AM
2025-01-07 4:01 AM
"I'm quite new to C++ so I may have made a few errors. "
The code does not build. Please fix it.
\Digital_scroll\TouchGFX\gui\src\screen1_screen\Screen1View.cpp(9,55): error C2039: 'scrollWheel11AnimateToHandler': is not a member of 'Screen1View
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.