STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

If STM QVGA display support touch keyboard

Hello sir,                           For my project using the STM32F429I-DISC1 board, I need to implement English, Spanish, and German keyboard layouts. Are these layouts pre-configured, or do I need to customize them? If customization is needed, wha...

balaji_s by Associate II
  • 1311 Views
  • 2 replies
  • 0 kudos

Model-View-Presenter

Hi everyone,I’ve been trying to implement a mechanism to save two matrices (each containing values of type Unicode::UnicodeChar*) and an errorCount variable using the Model-View-Presenter (MVP) architecture in TouchGFX. The issue arises when transiti...

AS5 by Associate II
  • 1781 Views
  • 1 replies
  • 0 kudos

Resolved! RVA15MD + NUCLEO-C071RB

Good morning,we are trying to program a RVA15MD + NUCLEO-C071RB display. When loading the TouchGFX Demo 4 the programming is not successful (see errors in the attachment). While with the TouchGFX Demo 8 everything loads correctly and the demo works.C...

Error Programming Demo4 _RVA15MD + NUCLEO-C071RB.png

Resolved! Shows wrong images of the buttons

Hello Gang.I have STM32U5G9J-DK2 discovery kit.Latest software, TouchGFX and ...CubeI am NOOB and may be do something wrong but I do not see any mistakes from my side.I did small test project in the TouchGFXBut after uploading it to the kit I got : I...

Screenshot 2025-01-19 at 22.29.11.png WhatsApp Image 2025-01-20 at 07.47.41_52a9f13b.jpg
dibor by Associate II
  • 3063 Views
  • 7 replies
  • 4 kudos

Resolved! RGB image compression memory fault

Hey,I am trying out the new RGB image compression in TGFX 4.24 and are having some issues. My program compiles fine without any compression.I have only turned the feature on in TouchGFX Designer and generated code. Is there something else I am missin...

PontusL by Associate III
  • 3966 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.