2020-11-19 11:02 PM
I redesign a layout of a keyboad (as I'm interested in numeric keys only, for a login).
Everything is OK but I didn't managed to place the text of the key inside its button shape
( i.e. texts: "1", "2", etc appears outside the button)
How can I tell where to draw the texts of keys?
Thanks
2020-11-20 6:23 AM
Hi,
What have you done exactly ? Are you using the keyboard example provided in TouchGFX Designer or a project of your own ?
Could you share some screenshots or some code ?
/Romain
2020-11-24 5:24 AM
I solved the problem in another way: I redesigned the layout from the ground up and wrote a class to handle my custom keyboard but it was a pity
having a working framework which already handles a quite generic layout and give up just because the keys text appear not centerd respect to the keys itselves.
Anyway the original layout was:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.