2025-01-28 2:52 AM - edited 2025-01-28 4:38 AM
TouchGFX Simulator is not working and it doesn't give any error while creating code or running the simulator.
I created a new project I didn't even choose a board I tried it with the "Simulator"
I want to try some ui designs in TouchGFX. I created a new project in Simulator type:
I just added a white box:
I generated code:
Generate Code
Generate
Wrote generated/gui_generated/include/gui_generated/screen1_screen/Screen1ViewBase.hpp
Wrote generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Done
I clicked "Run Simulator":
Run Simulator
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Compile
make -f simulator/gcc/Makefile -j8
Done
Run
build\bin\simulator.exe
Done
Done
I tried to search for simulator.exe file in my project directory, but the file is not exist. I'm using 4.24.2 version now.
Since there is no error. I'm lost on debugging. Thx for help.
Solved! Go to Solution.
2025-01-29 11:14 PM
I was using it. I think the issue started after I updated the app.
2025-01-30 2:04 AM
There must be something different on your system.Do you have a virus scanner active? It might block the simulator.
If all else fails you can try installing TouchGFX in a virtual machine as a workaround.
2025-01-30 3:14 AM
I literally resetted the whole computer just to fix this...
And yes it works now. I do not know why that issue happened but after computer reset and re-installing TouchGFX Designer and Microsoft Visual C++ Redistributable Version from this link : https://learn.microsoft.com/en-us/cpp/windows/latest-supported-vc-redist?view=msvc-170
it works now. Thanks for helping!
2025-01-31 7:39 AM
@barisubasi wrote:I literally resetted the whole computer just to fix this...
Reset as in reboot or reset as in Fresh install of windows?
2025-02-03 12:50 AM
fresh install of windows. resetted everything. installed touchgfx again
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.