2021-01-25 9:10 AM
Hello,
this is not the first time i set touchgfx in a custom board (with STM32F767 MCU). I always followed the method described in the touchfgx documentation, which can be summarized in this video guide.
Now i'm trying to get it to work with STM32H743 MCU. I tested first the framebuffer in the internal and external ram respectively, following the official documentation. Once working, i enabled touchgfx 4.16 (i'm using CUBEIDE 1.5.1), i enabled CRC and FreeRTOS v2 and i inserted MX_TouchGFX_Process() inside the GUI Task.
When i debug it returns HardFault, but if i remove the MX_TouchGFX_Process() function it debugs without problems, but obviously nothing happens.
I tried to use __HAL_RCC_CRC_CLK_ENABLE(); before initializing Touchgfx, but nothing.
I also noticed that the "Generate Under Root" checkbox is checked and i can't uncheck it, while the official documentation says to uncheck it.
Cane someone help me?
Thank you.
Solved! Go to Solution.
2021-01-25 9:36 AM
2021-01-25 9:36 AM
2021-01-25 9:52 AM
How can i enable Dcache from CubeMX?
2021-01-25 10:01 AM
First menu SystemCore ... CORTEX M7
2021-01-25 10:08 AM
Ok, it works! Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.