2020-10-26 1:08 AM
Hi,
I'm trying to build and run the examples from TouchGFX Designer 4.15.0 on the STM32H7B3 Discovery kit and all I'm getting is a blank screen.
So I guess the basic question is should I be able to create, compile, program and run the examples directly out of TouchGFX Designer without (manually) opening any of the other applications?
If yes is there something I should check in TouchGFX settings or on the board to mmake this work or is it a bug in TouchGFX Designer?
Edit: Possibly it is not programming correctly though there is no indication of this in the detailed (Alt-L) log in TouchGFX Designer attempting to program the target.hex using STMCube32PRogrammer outputs the following:
08:42:35 : Opening and parsing file: target.hex
08:42:35 : File : target.hex
08:42:35 : Size : 2458468 Bytes
08:42:35 : Address : 0x08000000
08:42:35 : Erasing memory corresponding to segment 0:
08:42:35 : Erasing internal memory sectors [0 21]
08:42:35 : Erasing memory corresponding to segment 1:
08:42:35 : Erasing memory corresponding to segment 2:
08:42:35 : Download in Progress:
08:42:37 : Error: failed to download Segment[2]
08:42:37 : Error: failed to download the File
08:42:37 : RUNNING Program ...
08:42:37 : Address: : 0x08000000
Looking at the Write protection flags in the Option Bytes they are all ticked which indicates not active.
Solved! Go to Solution.
2020-11-02 9:55 PM
The new version of the H7B3-DK AT is now online. It's the v3.0.3.
Can you select it along with a UI example, run target and tell us if it's working for you ?
/Alexandre
2020-10-26 6:52 PM
Hello,
The issue with the H7B3-DK Application Template is known by the development team. We will try to fix it as soon as possible.
Sorry for the inconvenience,
/Alexandre
2020-10-27 12:51 AM
Thanks for letting me know, is there any ETA? Is there anywhere I can get a notification (here or by subscribing somewhere else)? Does it work with an older version, if so can you tell mw which version? Thanks, Martin.
2020-10-29 10:00 PM
I will come back to you on this thread when I know the fix is online.
/Alexandre
2020-11-02 9:55 PM
The new version of the H7B3-DK AT is now online. It's the v3.0.3.
Can you select it along with a UI example, run target and tell us if it's working for you ?
/Alexandre
2020-11-02 11:36 PM
Yes I'll try it. Yesterday I was trying older versions, uninstalled them all, redownloaded v4.15.0 and installed that and it seems to be working for me. So possibly I downloaded it already how do I determine which AT version I have?
2020-11-02 11:38 PM
Nevermind I see the version in the info for the template I have v3.0.3 and can confirm it is now working, thanks Martin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.