2023-12-12 9:41 PM
I'm using the stm32h750-dk development board and TouchGFX 4.21.4 and STM32CubeIDE. I want to design a circular progress bar with a color gradient. I attached the required circular progress bar as an image. so I want to control the circular progress bar from the main.c using an external variable resistor. I'm Using the 'queue' to communicate between touch TouchGFX files and main.c file. Still, I can control the progress bar using a single color (without a color gradient). anyone can help me to implement a circular progress bar with a color gradient when progressing the bar.
this is the code that I use now.
2023-12-15 2:32 AM
Hello @sandaruwan,
Unfortunately, there is no direct way to do it, and I don't have any solid ideas for doing it right now. But, I think if you use an image with gradient as your progress indicator, you might be able to get close to what you look for.
I will update you if I found a solution.
Best regards
2023-12-15 8:58 AM
Thanks your response @Mohammad MORADI ESFAHANIASL . please let me know if you find any solution. not possible to use images with gradient because the gradient area is dynamically changing with the progress value.
2023-12-18 1:56 AM
I see. I will surely update you
Good luck
2024-08-02 8:48 AM
I came here for a different reason and this was the exact same thing I though about when I saw the post.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.