2023-05-04 12:05 AM
Hello,
I use ToucheGFXDesigner 4.21.3 for the first time.
I have no problem to design the application for the 2 buttoms Run Simulator and Run Target are not Highlitghted. When, I point these buttoms, it's written : Can't run Simulator and Can't run target. Samething in the menu Code
I probably miss something but what?
If somebody coul help ?
Best Regards
Robert
2023-05-06 10:29 AM
Hello. Good that you get forward :thumbs_up: I dont have ideas about deleting 4 files, maybe somebody else can help you, maybe somebody have use TGFX with Win 11.
2023-05-06 11:58 PM
Hello JTP,
For your information, the issue is solved.
After your idea to cancel the 4 blocking files, I was able tu run completly TouchGFX with any project.
Then, I try to run in Stm32CubeIde. When, I open the .ioc file, the system ask for a major update (1GB). Everything was fine, I started to debug. The system ask for a firmare update of the Stm32LINK probe ( included in the board).
After that, I run the project from Stm32CubeIde. Everything was fine and the demo is perfect on the board.
Then, I redo the TouchGFX simulation. The 4 blocking files are no more blocking.
My understanding now is the firmware update of the Stm32LINK probe is the key point.
Thanks again for your support
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.