2023-05-04 12:05 AM
Hello,
I use ToucheGFXDesigner 4.21.3 for the first time.
I have no problem to design the application for the 2 buttoms Run Simulator and Run Target are not Highlitghted. When, I point these buttoms, it's written : Can't run Simulator and Can't run target. Samething in the menu Code
I probably miss something but what?
If somebody coul help ?
Best Regards
Robert
2023-05-04 2:27 AM
Hello. I think you have some error in screen 2 buttonWithLabel because it has yellow tab. Fix that first.
2023-05-04 9:52 AM
Hello,
Thanks for answer. You are right, I have not understood, there was a mistake.
Now, Simulator and run target buttoms work well
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.cproject file: ../../STM32CubeIDE/CM7/.cproject
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.project
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.cproject
Done
Compile
make -f ../../gcc/Makefile clean && make -f ../../gcc/Makefile -j8
make -C C:/TouchGFXProjects/MyApplication_2/gcc/ -f makefile_cm4 clean
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_2/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_2'
Cleaning: STM32H747I_DISCO
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_2'
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_2/gcc'
make -C C:/TouchGFXProjects/MyApplication_2/gcc/ -f makefile_cm7 clean
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_2/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_2'
Cleaning: STM32H747I_DISCO
rm: cannot remove `CM7/TouchGFX/build/bin/libjpeg-8.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/SDL2.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/SDL2_image.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/simulator.exe': Permission denied
make[2]: *** [_clean_] Error 1
gcc/makefile_cm7:462: recipe for target '_clean_' failed
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_2'
make[1]: *** [clean] Error 2
makefile_cm7:49: recipe for target 'clean' failed
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_2/gcc'
../../gcc/Makefile:10: recipe for target 'clean' failed
make: *** [clean] Error 2
Failed
Failed
Best Regards Robert
2023-05-04 11:49 AM
Hello. Are you running simulator same time when trying to update it target ? That prevents removing of those files.
2023-05-05 12:11 AM
Hello JTP,
I try with and without running simulator same time when trying to update it target. Same Issue
I also try the example : COVER TRANSITION. Same issue see below
The issue seems to be :
rm: cannot remove `CM7/TouchGFX/build/bin/libjpeg-8.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/SDL2.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/SDL2_image.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/simulator.exe': Permission denied
I download the touchGFX directly from ST site. Is it better to download from STM32Cube IDE ?
Best regards
Robert
------------------------------------------------------------------------------
COVER TRANSITION
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.cproject file: ../../STM32CubeIDE/CM7/.cproject
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.project
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.cproject
Done
Compile
make -f ../../gcc/Makefile clean && make -f ../../gcc/Makefile -j8
make -C C:/TouchGFXProjects/MyApplication_4/gcc/ -f makefile_cm4 clean
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
Cleaning: STM32H747I_DISCO
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make -C C:/TouchGFXProjects/MyApplication_4/gcc/ -f makefile_cm7 clean
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
Cleaning: STM32H747I_DISCO
rm: cannot remove `CM7/TouchGFX/build/bin/libjpeg-8.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/SDL2.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/SDL2_image.dll': Permission denied
rm: cannot remove `CM7/TouchGFX/build/bin/simulator.exe': Permission denied
make[2]: *** [_clean_] Error 1
gcc/makefile_cm7:462: recipe for target '_clean_' failed
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
makefile_cm7:49: recipe for target 'clean' failed
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[1]: *** [clean] Error 2
../../gcc/Makefile:10: recipe for target 'clean' failed
make: *** [clean] Error 2
Failed
Failed
2023-05-05 4:30 AM
Can you delete those files manually from windows file manager ? Do you have permissions for it in windows in that folder.
2023-05-05 6:56 AM
Hello JTP,
Thanks for your support. I have administrator permissions but I don't know where are these files.
Best regards
PS. My system is windows 11
2023-05-05 9:48 AM
Hello. In your case files seems to be in
C:\TouchGFXProjects\MyApplication_2\CM7\TouchGFX\build\bin or MyApplication_4
folder. Those 4 files are generated when simulator build is make. This problem can be win11 related, I havent test TGFX in win11 and i'm not sure is it even officially supported OS.
2023-05-05 11:38 PM
Hello JTP,
Thanks for this new idea. I erase all these files.
A lot of progress but the Run Target fail. Reason : c:/TouchGFXProjects/MyApplication_4/gcc/include/flash_sections_int_ext.mk:4: recipe for target '_intflash_' failed
Best regards
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.cproject file: ../../STM32CubeIDE/CM7/.cproject
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.project
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.cproject
Done
Compile
make -f ../../gcc/Makefile clean && make -f ../../gcc/Makefile -j8
make -C C:/TouchGFXProjects/MyApplication_4/gcc/ -f makefile_cm4 clean
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
Cleaning: STM32H747I_DISCO
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make -C C:/TouchGFXProjects/MyApplication_4/gcc/ -f makefile_cm7 clean
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
Cleaning: STM32H747I_DISCO
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make: 'Makefile' is up to date.
Done
Flash
make -f ../../gcc/Makefile flash
make -C C:/TouchGFXProjects/MyApplication_4/gcc/ -f makefile_cm4 flash
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
make[3]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_cortex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_crc.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_crc_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma2d.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dsi.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_exti.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_gpio.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_hsem.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_i2c.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_i2c_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_ltdc.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_ltdc_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_mdma.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pwr.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pwr_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_qspi.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_sdram.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim_ex.c
Compiling Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_ll_fmc.c
Compiling CM4/Core/Src/main.c
Compiling CM4/Core/Src/stm32h7xx_it.c
Compiling CM4/Core/Src/stm32h7xx_hal_msp.c
Compiling STM32CubeIDE/CM4/Application/User/Core/syscalls.c
Compiling STM32CubeIDE/CM4/Application/User/Core/sysmem.c
Compiling Common/Src/system_stm32h7xx_dualcore_boot_cm4_cm7.c
Compiling ASM STM32CubeIDE/CM4/Application/User/Startup/startup_stm32h747xihx.s
Linking CM4/TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
make[3]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_4'
-------------------------------------------------------------------
STM32CubeProgrammer v2.3.0
-------------------------------------------------------------------
ST-LINK SN : 003E00463431511237393330
ST-LINK FW : V3J10M3
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x450
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
Memory Programming ...
Opening and parsing file: intflash.hex
File : intflash.hex
Size : 3444 Bytes
Address : 0x08100000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 8
Error: failed to erase memory
Error: failed to erase memory
Hard reset is performed
c:/TouchGFXProjects/MyApplication_4/gcc/include/flash_sections_int_ext.mk:4: recipe for target '_intflash_' failed
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_4'
make[2]: *** [_intflash_] Error 1
makefile_cm4:42: recipe for target 'flash' failed
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_4/gcc'
make[1]: *** [flash] Error 2
../../gcc/Makefile:10: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed
///////////////////////////////////////////////////////////////////////////////////////////
2023-05-05 11:55 PM
Hello JTP,
I did a second time, it works well.
Many tanks. Now, Why these 4 files are not working ?
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.