2020-04-01 10:30 AM
Hi,
I have working on below setup:
Software Tool Chain:
STM32CubeMX 5.6.0
TouchGFX 4.13.0 Designer
STM32CubeIDE 1.2.0
Hardware:
STM32F746G-DISCO (Discovery Board)
I have created GUI on TouchGFX 4.13.0. worked fine on simulator and Discovery Board as well.
But I am trying import and open project in STM32CubeIDE 1.2.0.Imported Successfully . But Project not successfully compiled.
22:34:33 **** Clean-only build of configuration Release for project STM32F746G_DISCO ****
make -j4 clean
rm -rf *
rm: can't remove 'Middlewares/ST/touchgfx': Directory not empty
make: [makefile:151: clean] Error 1 (ignored)
22:34:36 Build Finished. 0 errors, 0 warnings. (took 2s.371ms)
22:34:40 **** Build of configuration Release for project STM32F746G_DISCO ****
make -j4 all
In file included from ../TouchGFX/simulator/main.cpp:1:0:
../../Middlewares/ST/touchgfx/framework/include/platform/hal/simulator/sdl2/HALSDL2.hpp:22:10: fatal error: SDL2/SDL_video.h: No such file or directory
#include <SDL2/SDL_video.h>
^~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [TouchGFX/simulator/subdir.mk:18: TouchGFX/simulator/main.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j4 all" terminated with exit code 2. Build might be incomplete.Please Check attachment...and update ..
I have add/use to USB Mass Storage Stack , SDMMC with FATFS with TouchGFX GUI .
--
Karan
Solved! Go to Solution.
2020-04-30 3:29 AM
Hi Karan,
Your problem is that CubeIDE is trying to compile SDL2 files (simulator). Newest version of CubeIDE and latest version of the AT should not have this issue. Can you verify?
/Martin
2020-04-30 3:29 AM
Hi Karan,
Your problem is that CubeIDE is trying to compile SDL2 files (simulator). Newest version of CubeIDE and latest version of the AT should not have this issue. Can you verify?
/Martin
2020-04-30 5:21 AM
Thanks for response .. But Problem already solved with Below Toolchain..
STM32F746G Discovery Kit v3.0.1
STM32CubeMX 5.6.0
TouchGFX 4.13.0 Designer
STM32CubeIDE 1.3.0
Anyway Thanks..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.