STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Show a custom container on the screen

Hi everyone,I created a custom container and I created a button, so I want to fade the custom container on the screen when I click the button!i created a virtual function within TouchGFX then I created an object of my custom contain class inside this...

idrissmc by Associate III
  • 1386 Views
  • 2 replies
  • 0 kudos

STM32469I-EVAL DSI read

Posted on November 11, 2016 at 21:25Hello,I am trying to test the DSI HAL but am having trouble making the read function work on the LCD screen included in the kit.Here is my attempt to execute a get_address_mode request.HAL_StatusTypeDef status = H...

lthiery by Associate II
  • 2242 Views
  • 5 replies
  • 0 kudos

II have STM32F7508-DK, I would like to integrate TouchGFX with STM32CUBE IDE, but it is not working, I am searching instructions or, even better, a tutorial. Thank you very much.

I have the development kit, I made an application, following an ST tutorial, but it is still not working. I have the .bin file, but when I debug the program the display doesn't show anything, and the red led continuos blinking, I think there are some...

LMalv.1 by Associate II
  • 2890 Views
  • 5 replies
  • 0 kudos

Does Drawable::invalidateRect need a non-const rect?

I've come up with the following issue while trying to invalidate an area. I would expect that I could grab a MinimalRect from an object and pass it directly to the base container, as the following:invalidateRect(arc.getMinimalRect());However, I get ...

j o by Associate II
  • 1537 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.