2020-10-27 7:06 AM
Hello,
I'm currently developing an application on a STM32H753VT6 with touchGFX and I have an issue with textAreas. Just to say that I'm using my personnal font ( size : 20/24/34 px). Each textArea has just one wildcard with a 17 chars size buffer. I'm sending text through a terminal on my PC to change wildcards values.
In some cases, I don't know when, one letter is not totally displayed even if I invalidate all possible areas. Here are some pictures to illustrate the problem :
As you can see, it is always the second character that is partially displayed (but sometimes there is no problem, for example, adding a space " " before "APPEL EN COURS" works)
Any idea ?
Regards,
AJT
Solved! Go to Solution.
2020-11-09 12:36 AM
2020-10-28 4:14 AM
Hi,
Could you share your font and your code handling the texts? Does that issue happen with other fonts as well?
/Romain
2020-10-28 4:52 AM
Hello,
Here there are.
Search when strncpy function is used in cpp files to see where texteAreas are updated
And yes I've juste tried with the Courier New Font (size : 34) and I have the same problem with 16 W (the 2nd one is not totally displayed) (test done for the the call in progress screen)
Thnks again,
AJT
2020-11-09 12:36 AM
2024-05-14 3:29 AM
Hi there
I have been trying to follow the above link, as I am experiencing the same problem, with parts of text appearing erased. However, when I click on the link given, I get:
"An invalid set of parameters has been specified in the url."
Could you please repost a valid link (I know that the original one is a few years old now)?
Many thanks,
John
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.