2024-04-20 4:10 AM
Hello everyone.
I have my custom board.
STM32F750Z8 CPU with MT25QL128ABA External Flash.
I don't have external RAM.
My application code runs at External Flash. It is a simple code. I create just one screen at the TouchGFX and add two buttons. No other screens, no interactions... It's very light code.
I try to communicate 4.3(480x272) TFT-LCD. But it doesn't show full screen. Bottom of the screen is missing. (Image attached).
I tried different "buffer addresses" like 0x20000000(DTCM) and 0x20010000(SRAM1). SRAM1 address is more reliable. I tried to change "Signal Polarity" but it didn't affect.
Thanks for helping.
CubeIDE version 1.6.1
TouchGFX version 4.16.0
Windows 7
Solved! Go to Solution.
2024-04-20 6:39 AM
Simple 320 Kbytes of SRAM (including 64 Kbytes of Data TCM RAM for critical real-time data)
480x272x3 oversized your ram. Use RGB565 or L8
2024-04-20 4:13 AM
2024-04-20 6:39 AM
Simple 320 Kbytes of SRAM (including 64 Kbytes of Data TCM RAM for critical real-time data)
480x272x3 oversized your ram. Use RGB565 or L8
2024-04-20 7:40 AM
Hi. Thanks for the response.
I got no error about "RAM Size". But i have tried RGB565 just incase. Nothing changed.
By the way, i know internal RAM is not enough for simple 480x272 image. That's why i used "box" instead of "image".
Surprisingly;
When i set RGB888, RAM Usage:49,35KB
When i set RGB565, RAM Usage:49,29KB
2024-04-20 9:22 AM
RAM is not counted when you choice config by address in touchGFX and RGB565 is not simple change . Primary you must change it in Layer 1 LTDC config not diplay config
2024-04-24 6:55 AM
@MM..1 Thanks for the replies. I was wrong about the Buffer size. Now it works with RGB565. I think I forgot to recompile TouchGFX project after I changed the RGB565 settings. That's why i got same error after RGB565 settings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.