2022-01-08 11:36 AM
I'm looking for some processors to achieve a couple tasks. First, I would like to get input from two cameras. The interface isn't important, I will find the cameras based on the processor. But then I want to also be able to send that video stream over WiFi, It's okay, if this will require two processor sets, as long as I can transfer the data from one to the other using something like FDCAN or some other internal, fast connection. I did look at the STM32MP line of processors, but they are a bit more expensive, and also much more capable than I require.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.