2019-11-28 7:10 AM
I'm porting toughgfx button example to rt-thread. I tested the environment with led blinking.
My environment is as below.
tool chains: scons + gas/gcc/g++
debugging : openocd + gdb
flash program : STM32CubeProgrammer with openjdk and openjfx
RTOS: rt-thread
Board: stm32f746g-disco
I merged the touchgfx button example into rt-thread. And then I began to experience a hard fault. It starts with touchgfx::touchgfx_init(). I checked that I have no problem with cpp codes, such as new operator and STL.
at touchgfx-button/Middlewares/ST/TouchGFX/touchgfx/framework/include/common/TouchGFXInit.hpp:86
86 HAL& hal = getHAL<HALType>(dma, display, tc, width, height);
at touchgfx-button/Middlewares/ST/TouchGFX/touchgfx/framework/include/common/TouchGFXInit.hpp:87
87 hal.initialize();
void OSWrappers::initialize()
0801c9a0 <_ZN8touchgfx3HAL10initializeEv>:
801c9a0: b510 push {r4, lr}
801c9a2: 4604 mov r4, r0
801c9a4: f7f2 f986 bl 800ecb4 <_ZN8touchgfx10OSWrappers10initializeEv>
801c9a8: 6860 ldr r0, [r4, #4]
801c9aa: 6803 ldr r3, [r0, #0]
801c9ac: 68db ldr r3, [r3, #12]
801c9ae: 4798 blx r3
After the call to OSWrappers::initialize(), r3 was 0x9db545a1.
801c9ae: 4798 blx 0x9db545a1
For your information, my lds file is...
================= lds file =================
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M
}
There should be no codes in QUADSPI area. But I don't know what that code is. Would you please advise me with my lds file?
I've enclosed the linker script file.
Solved! Go to Solution.
2021-02-25 7:13 AM
I had a hard fault error that came up when ever the external FLASH on a '469-Disco board was accessed. In the CubeIDE it looked like the data was in the FLASH -so what was the problem????
It turned out that STLINK could access the FLASH but the program couldn't. The clue to fixing this problem was the youtube https://www.youtube.com/watch?v=237lPdMsDZsL . I needed to copy files into the BSP folder for the touchscreen and QSPI FLASH which I copied from one of the demos. Also some of the parameters that CubeMX generated for the FLASH in the main.c appeared to be incorrect. These were replaced by the settings from the demo.
Hope this helps someone save some time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.