2019-01-27 1:03 AM
Hi , In TouchGFX designer I've added some custom C++ code to button interactions (something like "button.setState(!button.getState());" - simulation inside the Designer executes good, so I believe the code is not an issue).
Generation code was successful , simulation run inside Designer also succeeded.
But added C++ functionality was not as expected,so I decided to debug the execution code
I've opened "Application.sln" located in ProjectRoot/simulator/msvs directory .
Then tried to build ,solved text and images generation issues ,and in the end received linker error :
Error LNK2001 unresolved external symbol "public: __thiscall FrontendApplicationBase::FrontendApplicationBase(class Model &,class FrontendHeap &)" (??0FrontendApplicationBase@@QAE@AAVModel@@AAVFrontendHeap@@@Z) Application ProjectRoot\TouchGFX\simulator\msvs\FrontendApplication.obj 1
Error LNK2001 unresolved external symbol "public: void __thiscall FrontendApplicationBase::gotoScreen1ScreenNoTransition(void)" (?gotoScreen1ScreenNoTransition@FrontendApplicationBase@@QAEXXZ) Application ProjectRoot\TouchGFX\simulator\msvs\main.obj 1
Error LNK1120 2 unresolved externals Application ProjectRoot\TouchGFX\build\Release\bin\Application.exe 1 Tried in Visual Studio Community and Professional 2017 under Windows 10 x64 and Windows 7 x64 ,with Microsoft SDK v141. Received same error for Debug and Release configurations .
The above mentioned files (FrontedAppication.hpp , FrontedHeap.hpp) located (from VS 2017 Solution Explorer perspective) in "Header Files/gui/common" directory .
The "FrontedApplication.cpp" located in "Source Files/gui/common"
If somebody faced similar problem, help will be appreciated.
Solved! Go to Solution.
2019-01-27 1:31 AM
Problem solved with :
provided by
@Anders Nedergaard PETERSEN
2019-01-27 1:31 AM
Problem solved with :
provided by
@Anders Nedergaard PETERSEN
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.