2015-11-16 11:21 PM
Hi,
I am working onSTM32F429 for LCD interface (LTDC).
LCD controller: ILI9341
Interface used: RGB
We are using STemWin li
brary for GUI interface.
We are able to work with GUIDRV_FLEXCOLOR_F66709 setting for 16 bit parallel interface.
But we could not map PortAPI parameters
(write16 bit data and read16bit) for GUIDRV_FlexColor_SetFunc() with RGB interface.
Can we use the GUIDRV_FLEXCOLOR_F66709
for RGB interface? If not, which should be setting for RGB interface?
Thanks in Advance.ByTamilselvan #stemwin #ili9341 #ldtcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.