2019-06-06 3:39 AM
Hello,
in STM32F746 DISCO.
Microsd detect pin is : PC13
LCD touch interrupt is : PI13
how to make use of both interrupts in the application ?
Solved! Go to Solution.
2019-06-06 4:00 AM
The short answer is "you can't". At least not using EXTI interrupt.
So how might you achieve the desired result instead?
PC13 happens to be RTC_TAMP1, so you could enable and use the corresponding RTC interrupt, leaving EXTI13 wired to PI13.
Or, since (in my experience) it takes quite a long time to mount a microSD card once it is inserted, maybe the detection of its insertion could be delayed by (say) up to 100 ms. In that case all you need do is poll PC13 in software every 100 ms. I suspect some real-time operating-systems make this fairly easy. But you could also do this in response to a timer interrupt.
Hope this helps,
Danish
2019-06-06 4:00 AM
The short answer is "you can't". At least not using EXTI interrupt.
So how might you achieve the desired result instead?
PC13 happens to be RTC_TAMP1, so you could enable and use the corresponding RTC interrupt, leaving EXTI13 wired to PI13.
Or, since (in my experience) it takes quite a long time to mount a microSD card once it is inserted, maybe the detection of its insertion could be delayed by (say) up to 100 ms. In that case all you need do is poll PC13 in software every 100 ms. I suspect some real-time operating-systems make this fairly easy. But you could also do this in response to a timer interrupt.
Hope this helps,
Danish
2019-06-06 4:07 AM
Hello Danish,
Great insights . Thanks for the clarification .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.