2018-12-24 10:24 PM
Hi
Another problem with Animated Image example at win 10
log file is enclosed ,
I could run the same example at win 7
Can anybody help
2019-01-02 4:03 AM
Can you share your project? I would like to try it on my own machine here.
Thanks!
2019-01-02 4:07 AM
How ?
zipped Project folder is more than 20MB
any other way to share project with you?
2019-01-02 4:17 AM
Do you have an external file sharing option, like dropbox, you can use? Otherwise i will try to set something up. You could also prune your zip file a bit - The build folder, for instance, could be removed.
Any .o files and the touchgfx folder itself could be removed. I'll put in the touchgfx folder myself.
2019-01-02 4:22 AM
This could be an issue related to the way i's are handled in Turkey. That's where you're based, right?
The images in your assets folder are called "ani_0x.png". Could you rename these to something that does not contain "i", but retain the order (_00.png, _01.png, etc)
Thanks!
2019-01-02 4:25 AM
If that's the case, then i'll file a bug report with the design team.
You could try creating a custom application using any image that contains an "i" and see if you don't get the same error.
2019-01-02 4:56 AM
I tried a new project with blank UI and "error during code generation " again
I renamed ani_0x.png files at assets folder and reopen project
":animation image ani_14.png does not exist"
I live in Istanbul
2019-01-02 5:06 AM
Okay, if you have the same issue with a blank application, then it should have nothing to do with the image file names. I forgot to add that when you rename the images, you have to instruct the designer to use a different range of images in the properties of the animated image.
2019-01-02 5:07 AM
When you say you also have issues with a blank application, what is the error then? Can you share the log? Because the log from the AnimatedImage example had references to the AnimatedImage component where as this application would probably have a different kind of error.
Thanks!
2019-01-02 5:08 AM
Okay, if you have the same issue with a blank application, then it should have nothing to do with the image file names. I forgot to add that when you rename the images, you have to instruct the designer to use a different range of images in the properties of the animated image.
(STMicroelectronics)
Okay, if you have the same issue with a blank application, then it should
have nothing to do with the image file names. I forgot to add that when you
rename the images, you have to instruct the designer to use a different
range of images in the properties of the animated image.
Hi Martin Thank you for your answer
error window enclosed
[image: jpg]
touchgfx error
(Asis Otomasyon)
I tried a new project with blank UI and "error during code generation "
again
I renamed ani_0x.png files at assets folder and reopen project
":animation image ani_14.png does not exist"
I live in Istanbul
(STMicroelectronics)
Okay, if you have the same issue with a blank application, then it should
have nothing to do with the image file names. I forgot to add that when you
rename the images, you have to instruct the designer to use a different
range of images in the properties of the animated image.
.
Are notifications about this post getting annoying? Reply to this email
with the word " mute ".
STMicroelectronics N.V.
[image: ST Community]
2019-01-02 5:17 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.