2020-04-30 12:15 AM
We are using stm32H743
We need a frame buffer of 150K to our LCD. we do not have an external RAM, so we use the 412K internal RAM.
We also work with USB (Full speed mode).
each peripheral work on it own , but not together. if we enable both of them they are not working not even if the USB buffers are in another RAM section.
there isn't any compilation or linking error, but nothing is working on the board.
We think it can be stack or heap problem, but we do not manage to enlarge them without crashing.
we asked you this question before and you told us to increase the size of heap and stack but its didnt help
d you have another idea for us?
Thanks
2020-04-30 12:36 AM
I'm using LTDC and USB host at the same time on the H743 without any issues. Framebuffer is the 512K memory and is only used for that. I attach my load file if it helps
/*
*****************************************************************************
**
** File : LinkerScript.ld
**
** Abstract : Linker script for STM32H743ZITx Device with
** 2048KByte FLASH, 128KByte RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
** (c)Copyright Ac6.
** You may use this file as-is or modify it according to the needs of your
** project. Distribution of this file (unmodified or modified) is not
** permitted. Ac6 permit registered System Workbench for MCU users the
** rights to distribute the assembled, compiled & linked contents of this
** file as part of an application binary file, provided that it is built
** using the System Workbench for MCU toolchain.
**
*****************************************************************************
*/
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = 0x20020000-0x10; /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x1000; /* required amount of heap */
_Min_Stack_Size = 0x5000; /* required amount of stack */
/* Specify the memory areas */
MEMORY
{
DTCMRAM (rw) : ORIGIN = 0x20000000, LENGTH = 128K
AXIRAM (rw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (rw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (rw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
FLASH2 (r) : ORIGIN = 0x08100000, LENGTH = 1024K
RAM_D5 (rw) : ORIGIN = 0x38800000, LENGTH = 4K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >ITCMRAM AT> FLASH
/* used by the startup to initialize data */
_siDTCMData = LOADADDR(.DTCMData);
.DTCMData : {
. = ALIGN(4);
_sDTCMData = .; /* create a global symbol at DTCMData start */
. = ALIGN(4);
*stm32h7xx_it.o (.data .data*)
_eDTCMData = .; /* create a global symbol at DTCMData end */
} >DTCMRAM AT> FLASH
/* Uninitialized DTCM data section */
. = ALIGN(4);
.DTCMbss : {
. = ALIGN(4);
_sDTCMbss = .; /* create a global symbol at DTCMbss start */
. = ALIGN(4);
_eDTCMbss = .; /* create a global symbol at DTCMbss end */
} >DTCMRAM
/* used by the startup to initialize data */
_siITCM = LOADADDR(.ITCMSection);
.ITCMSection : {
. = ALIGN(4);
_sITCM = .; /* create a global symbol at ITCM start */
*stm32h7xx_it.o (.text .text*)
*stm32h7xx_it.o (.rodata .rodata*)
*Timers.o (.text .text*)
*Timers.o (.rodata .rodata*)
*stm32h7xx_hal_ltdc.o (.text .text*)
*stm32h7xx_hal_hcd.o (.text .text*)
. = ALIGN(4);
_eITCM = .; /* create a global symbol at ITCM end */
} >ITCMRAM AT> FLASH
/* The program code and other data goes into FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data goes into FLASH */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
.ARM : {
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} >FLASH
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} >FLASH
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} >FLASH
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} >FLASH
/* used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >DTCMRAM AT> FLASH
.my_section (NOLOAD):
{
. = ALIGN(4);
_s_my_section = .;
*(.my_section)
. = ALIGN(4) ;
_e_my_section = .;
} > DTCMRAM
/* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >DTCMRAM
/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
_e_endheap = .;
} >DTCMRAM
.backup (NOLOAD):
{
. = ALIGN(4);
_s_backup = .;
*(.backup)
. = ALIGN(4) ;
_e_backup = .;
} > RAM_D5
/* Remove information from the standard libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.